Hi,
I wanted to use the SD feature on TMS320DM36x DVRRD Rev2.1B board.
The board has not the SD slot. I expanded the SD slot to SD0 interface. (The SD0/1 has not the detect pin.)
I used the DM368_DVRRDK_v2.1 package. The UBL and U-boot of SD boot card could…
Part Number: DM8107 For a new project that needs DVR functionality and TI's DM8107 DVR Reference Design suits our requirement. Please refer the following link.
http://www.ti.com/tool/DVRRD?DCMP=DSP_dvr&HQS=dvr
Have a few queries on this
In case…
Part Number: TMS320DM8168 Hi Team:-
What I'm specifically looking for is a DVR reference design, and I noticed this one although it does look like it might be going obsolete (no further SDK releases etc): http://www.ti.com/tool/DVRRD
An off-the-shelf…
Hi Brad,
You can use EZSDK or DVR RDK for DM816x device. You can search in e2e forum regarding differences between EZSDK and DVR RDK, there is lot of info.
See also the below links:
processors.wiki.ti.com/index.php/DM816x_Design_Resources
http://www…
Part Number: TMS320DM8168 Hello,
Is it possible to do the following with dm816x:
1. record video + graphics (qt application)
2. change input from pal/ntsc in runtime
Which framework should be used for that ( dvrrd /eszsdk/other) ?
Thank you,
Ran
Part Number: TMS320DM8148 Hello,
Is it possible to do the following with dm814x:
1. record video + graphics (qt application)
2. change input from pal/ntsc in runtime
Which framework should be used for that (dvrrd/eszsdk/other) ?
Thank you,
Ran
Hi, all
My Version DVRRD K4.00.0.1 , DM8168; and I use REL.500.V.H264AVC.E.IVAHD.02.00.04.01 for encoding h264.
my question is : How to generate the SPS/PPS info in H264enc?
Thanks!
Hi, all
My Version DVRRD K4.00.0.1 , DM8168; and I use REL.500.V.H264AVC.E.IVAHD.02.00.04.01 for encoding h264.
my question is : How to generate the SPS/PPS info in H264enc?
Thanks!
Thanks shiju,
The problem was due to u-boot. we used u-boot of GA3.5 RDK & now the demo is working fine.
BTW, we are using DM8107 DVRRD Rev0.2B.
Thanks,
shashank.
Hi Badri,
Thanks for the prompt reply.
yes we are using UD DVR. The Board version is "DM8107 DVRRD Rev0.2B"
The details of FAE & sales person is as under,
mitesh@ti.com amar@ti.com
Thanks,
shashank.