Part Number: EK-TM4C1294XL Hi,
I want to read 3 analog voltage signals in an experiment. I want to implement this with the EK-TM4C1294XL part without any additional hardware. From what I have read in the datasheet, it seems so, because it consists of…
Part Number: EK-TM4C1294XL Other Parts Discussed in Thread: DCH010505S , We need the 3D models to add in our Philips library. the models in any universal format like step file.
DDR TERMINATION MODUL 15A 5V
Switched Supply Unit
PTH05010YAZ
MOD DC-DC…
Part Number: EK-TM4C1294XL Other Parts Discussed in Thread: TMS570LS1224 , EK-TM4C123GXL , UNIFLASH Hi, I'm trying to download demo examples through LM FlashLoader after uploading CAN Bootloader example (Uart to CAN, boot_can) to 2 EK-TM4C1294XL boards…
Part Number: EK-TM4C1294XL Dear all
Looking for a MQTT client library to work with our driver product which is based on the MCU, just wonder whether there is any example - noticed a CCS_SDK with some MQTT support in it? wonder whether it is good to move…
Part Number: EK-TM4C1294XL Other Parts Discussed in Thread: ENERGIA , TM4C1294NCPDT I'm starting a project with EK-TM4C1294XL, using ENERGIA IDE, I have flashed a test code sending SPI messages, and I can see the SPI frames(so code is running), but…
Part Number: EK-TM4C1294XL Other Parts Discussed in Thread: TPS2052B Hi,
I am thinking of using the EK-TM4C1294XL microcontroller for an application, and I would like to know if there is any way to supply 5 V (800 mA) from some output of the micro.
Thanks…
Part Number: TM4C1294NCPDT Other Parts Discussed in Thread: EK-TM4C1294XL
Hi, I'm trying to optimize the SPI timing and my goal is to have a continuous clock frame without any pause between bytes. I use EK-TM4C1294XL to do my tests. The SSI is configured…
Part Number: EK-TM4C1294XL Hi,
We configured the ccs project to do unit test (using parasoft).
while generating the test suits and test cases .
/resized-image/__size/1200x426/__key/communityserver-discussions-components-files/908/2273.ERROR.png
bellow…
Hi Seongwoong ,
I am not an expert with the 'EK- TM4C1294XL' controller. I can only provide assistance with TMS570LS1224 controller. If you share "TMS570LS1224" controller code, then i can validate and can confirm whether it is all good or…
Part Number: EK-TM4C1294XL I am trying to set the USB serial number using the sample program [usb_dev_cserial]. However, when I look at the device manager, I cannot find the serial number "12345678" set in g_pui8SerialNumberString. How do I…