Hello,
Can someone please tell me the register setup (or process) in order to receive data on the USB controller (Device mode). I'm using the EKI-LM4F232 development board.
I'm able to get past the setup stage, I'm also able to transmit data, but…
Hello!
On the photo at EKI-LM4F232 page ( http://www.ti.com/tool/eki-lm4f232 ) there are 4 apertures in the board corners. But in the actual device, that I use there are not. So my question is could I drill it without any damage for the board?
Thanks, Alex…
Why there's no option to view FPU registers while debugging using EKI-LM4F232 on board jtag. Using external J-link or simulator the view of FPU Register is available
Hi all,
We are working on getting all of our web pages in order for our recent launch of the Cortex-M4F products. We are still working on getting the software on the Software Updates page, but in the interim, please use the following links to download…
Hi Enrique,
I reposted this issue below and thanks for reply. Actually want to have the GUI widget scalier grid well buffered data dump into an Excel file such as the EKI-LM4F232 logger is able to do, assumed it to be using a USB port. XDS100v2 emulator runs…
Other Parts Discussed in Thread: TM4C123FH6PM Hi,
We bought Stellaris one EKI-LM4F232 Eval Kit and we've been programing it without problem.
Now we are assembling our own board using TM4C123FH6PM. We didn´t have any problems until I changed my code…
Other Parts Discussed in Thread: INA198 Hi, guys!
I was doing some measurements and I've noticed that the power consumption of LM4F232 on a EKI-LM4F232 board drops when set to 50 MHz. I've tested it on five boards and go the same results. Take a look see…
Hi Aaron,
We are using the EK-LMF4232 evaluation board, as shown in this link : http://www.ti.com/tool/eki-lm4f232
We have not tried the TM4C123 patch programmer, thinking that the support for the LM4F232H5QD has been discontinued after 1.10.1 firmware…
Another question on evaluation kit EKI-LM4F232 .
Included in the documentation is application note AN01272. It doesn't do anything other than reference source code which does not appear to be included and which all references appear to be dead.
Where…
I have an EKI-LM4F232 evaluation kit. It is noted in the description it is supposed to include code examples. I'm not expecting a lot from them but I'd at least like to puruse them. I don't see them on either the included CD or USB stick. …