David,
We do test our device very thoroughly, however not all of our software stacks are going to be ported to all platforms. In the case of SimpliciTI a decision was made not to create a port for the CC430Fx4x series.
When you browse to the tools folder…
And first one at https://www.ti.com/tool/MSP-FET is ...
Related design resources - Hardware development - EVALUATION BOARD - EM430F6147RF900
The EM430F6147RF900 development board supports all CC430F614x and flash parts in the 64-pin QFN (RGC) package…
Hi Bhavdipsinh,
The CC430F6147 is an active device and is fine to use in new designs. Although obsolete there are still a few distributors who have the EM430F6147RF900 available, or you can build your own using the Gerber files provided: www.ti.com…
Hello
Thank you very much for your reply~!!! >""<
I tset one EM430F6147RF900 board to send a packet to another EM430F6147RF900 board
my program can work in this case
but when i use one EM430F6147RF900 board to send a packet to the circuit…
hi
I want to buy the 868/915 MHz antenna
just like the same type antenna in EM430F6147RF900 Development Tool
but where can i find the manufacturers?
can anyone give a solution?
I've used an external power supply to find the point of failure.
3 EM430F6147RF900 identical dev boards were tested.
I've found out that the boards failed arround 2,68V-2.71V-2.78V (no difference between using SBW or JTAG).
I also found some…
Other Parts Discussed in Thread: CC430F6147 , CCSTUDIO How can I change the main voltage used for IO's (Vdd) on an eval board for a CC430? I'm using the board referenced from the part's webpage ( EM430F6147RF900)
It currently defaults to 3 V…
Hello I give you some detail description.
We find some of microcontrollers CC4306137, CC4306147 which have 1Ghz RF transceiver. Here below is the list of company which have EVM that full fills our requirements 1. Amber Wireless (http://www.ti.com/tool/msp430…
Other Parts Discussed in Thread: CC430F6147 , MSP430G2553 I'm trying to generate a square wave at 38 kHz on an output pin on a CC430F6147 (on the EVM EM430F6147RF900) . I'm doing this by simply toggling the pin in a timer interrupt of about 76 kHz. I…