Part Number: EVMASC-E99-B-50 Hello
I would like to get the design files of EVMASC-E99-B-50. I've got two eval boards and I need them
Could you help me, please?
thanks
Hi Mitch,
Thanks for the reply!
Mitch M said: Also, can you double check your setup to make sure the scope probes were not swapped? To me it looks like yellow is the output and blue is the input.
We have checked our set up and scope probes were not swapped…
Hi Sydney,
The auto calibration function is called from the DRV2605L_Q1_Init() function in which you can find the Haptic_EN_Set() function to make the enable pin high also i have added delay of 250ms in each function before making the EN pin low.
Please…
we want 1 circuit , 4 different current input and 4 mapped different current .
1 . can i used R=14.7K//14.7K ,0603,0.1W, to have 7.35K ?
2 . following are updated BOM is it ok sir?
Sr no.
Designator
Description
value
Tolerance
footprint
voltage
w…
Hi Rachel,
Are you seeing this issue on a TI EVM?
You could try increasing the TIFS communication timeout from 10s (default) to 100s just for testing purposes to see if that makes any difference:
diff --git a/drivers/firmware/ti_sci.c b/drivers/firmware…
Hi Judith ,
Thanks for informatoin,
If i configure as below in dts file , so can0 node is not showing.
root@am62xx-evm:~# ifconfig -a lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:250…
I now connected an external clock source and I am able to control the frequency. D1/D2 waveforms actually look good even at 250 kHz. Output current however improves only very very little, whereas going down in frequency decreases current capability very…
Hi Dominik,
Thanks for the revert and the update on the bug.
However I need clarifications on the following:
1) Is the bug only relevant to the constant current load? If it's not related to the type of load and only relevant to the coloumb counted capacity…
Hello Joe,
Thanks for the information.
I am guessing you see PART A only once, and it is when you press the button to load the array into the TX buffer?
Regarding Part B, what you are showing is one connection event with what probably are 4 packets of…
Other Parts Discussed in Thread: OPA380 Hello everyone,
I'am writing about simulation issue of OPA380 TI in Orcad Capture.
I tried to do simulation with pspice but the error is the following (in bold at the end):
-----------------------
Log file…