Part Number: EVMASC-E99-B-50 Hello
I would like to get the design files of EVMASC-E99-B-50. I've got two eval boards and I need them
Could you help me, please?
thanks
Part Number: TPS54360
Hi TI team ,
We are using the chip TPS54360DDAR for generating -24V input from +24V .Recently we have observed from field that TPS54360DDAR is Burning .its burning at Vin Pin (Pin no 2) and short B/w SW (Pin 8) and Gnd
Initially…
Part Number: TPS54360 Other Parts Discussed in Thread: LMR36015
Hi TI team ,
We are using the chip TPS54360DDAR for generating -24V input from +24V .Recently we have observed from field that TPS54360DDAR is Burning .its burning at Vin Pin (Pin no 2) and…
Other Parts Discussed in Thread: OPA380 Hello everyone,
I'am writing about simulation issue of OPA380 TI in Orcad Capture.
I tried to do simulation with pspice but the error is the following (in bold at the end):
-----------------------
Log file…
Hello David,
The code you gave me has "no PLL lock" error until I change "setupParams.fpgaRefClk = 500" and "sysParams.FRef = 500". Now PLL locks but produced SerDes error.
Here is the code that I used for your review. The…
Part Number: AFE7950 To support on AFE7950, LatteDebug1.docx
I have included a document that details some experimental cases on the AFE7950 that we executed this week with the LATTE software.
Case1 is the example design and it works as shown in the document…
Part Number: BQ27Z746 our battery use BQ27Z746 IC, after 2 months shipment, the batteries enter shutdown mode automatically and can't charge to exit , the communication result 、gg file and schematic shown as below, we need to find out why it can't…
Hi Juan,
Welcome to the E2E forum! The devices are the same, however the packaging differs. The ADS1115IGS T means the package is a small tape and reel of 250 devices whereas the ADS1115IGS R is a large tape and reel of 2500 devices.
Best regards,
Bob B …
Hi Wyatt
Thanks for your reply.
Attached the .gg file for your reference.
* Texas Instruments Data Flash File
* File created Thu Feb 22 16:49:25 2024
*
* Device Number 1E9B
* Firmware…
Hi Vaison,
The LMK05318 TICS Pro doesn't show DPLL calculation, I would recommend to use LMK05318 B TICS Pro so that you can see DPLL calculation is updated when changing PRIREF.
On the wizard page, make sure to set "Backward Compatible" so it can work…