Part Number: EVMASC-E99-B-50 Hello
I would like to get the design files of EVMASC-E99-B-50. I've got two eval boards and I need them
Could you help me, please?
thanks
hi,
It's a real R&D project for automotive and I am designing my own board with this driver. The board will have around 2500 leds so I will need two LP5891 drivers.
BR,
Javier Alvarez
Part Number: SN74LS00 Hi team,
I input quote API to create Quote, but resonance was 500.
would you please check it?
import requests
import json
# API keyとsecretからtokenを取得する
API_Key = 'lSSXG1QYnWwrKyAlMEOVTOMhoTfgw0lR'
API_Secret = 'wTVDeeGpeiufF64t…
Hi Sean,
Wanted to follow up on this thread. The main difference between LM61BIM3 X /NOPB and LM61BIM3/NOPB is the reel size in which the devices are shipped. LM61BIM3 X /NOPB comes in a large tape and reel which can hold up to 2500 devices. This orderable is…
Hello Dean,
yes I do have specific numbers. Please see the following table shows the five different setups we use for the two different ADCs. One of the setup (#3) is identical for both ADC types.
ADC type
Clk Setup
f(OSCin…
This is response from the api in create process
{
"orderInfo": {
"orderNumber": "T04780183",
"cartId": "C378942234",
"checkoutProfileId": ".....",
"currencyCode": "USD",
"orderDate": "2024-01-15T05:43…
Please, find attached Design Calculator V.8 that I did for your UCC14240-Q1 Schematic. I assumed a 30nC gate charge for your switch. The difference between V.6 and V.8 is that V.8 introduces the Cout1B capacitor connected between (VDD-VEE) at the gate…
Lets try to look at it one issue at a time.
You could 'Perhaps' connect the Mic direct to the ADC without using the PGA2500. Here we need to make sure that the input pin voltage on the ADC does not go above AVDD+0.3 v or below -0.3V . At these levels…
Hello David,
The code you gave me has "no PLL lock" error until I change "setupParams.fpgaRefClk = 500" and "sysParams.FRef = 500". Now PLL locks but produced SerDes error.
Here is the code that I used for your review. The…
With T designation INA220BIDGS ship at 250 parts per tape. package dimensions are Length :366.0 (mm), Width: 364.0 (mm), Height: 50.0(mm), at 9000 parts this will be 36 packages totaling Length : 366.0 (mm) Width: 364.0 (mm) Height: 1800(mm)
I agree with Clemens…