Part Number: EVMASC-E99-B-50 Hello
I would like to get the design files of EVMASC-E99-B-50. I've got two eval boards and I need them
Could you help me, please?
thanks
Hi Navadeep,
It won't be possible to generate 156.25 MHz, 40 MHz, 10 Mhz, and 122.88 MHz outputs at the same time with LMK05318B. Like the clock tree architect tool shows, 156.25 MHz and 10 MHz can both be derived from APLL1, since 2500 MHz is an integer…
Part Number: IVC102 We have performed 20 ABA test. When we take an old IVC102 from 2018/2020 and swap with an IVC102 from 2021/2023 the problem follows the IVC102.
Something has changed. The 10pF option has a much larger variation in measurement values…
Thank you all for the support.
We finally retested using a known/fast device as DK suggested. We used a WD My Passport SSD 1TB with dedicated Type-C port and NVMe technology.
With this device mounted in async mode, we are reaching 330 MBytes/s (around…
Part Number: DAC38RF82EVM I encountered difficulties in using DAC38RF8xEVM. After the JESD204b link was established, SYNC kept toggling, and DAC had no signal output.
Clock circuit adopts On-Board VCXO Clock Mode (CMODE4) in DAC38RF8xEVM to change the…
Part Number: DAC38RF82EVM Other Parts Discussed in Thread: DAC38RF82 , DAC38RF82 The SYNC signal is high when it is powered on I encountered a problem when debugging the DAC38RF82, as soon as the chip was powered on, it remained high without JESD204B link…
Part Number: BQ77904
we are keen on seeking additional assistance to tailor the BQ77904 ICS to our specific application, particularly catering to the LiFePO4 chemistry. Could we kindly request your support in modifying the product to align with the aforementioned…
Hello David,
The code you gave me has "no PLL lock" error until I change "setupParams.fpgaRefClk = 500" and "sysParams.FRef = 500". Now PLL locks but produced SerDes error.
Here is the code that I used for your review. The…
Hi Wyatt
Thanks for your reply.
Attached the .gg file for your reference.
* Texas Instruments Data Flash File
* File created Thu Feb 22 16:49:25 2024
*
* Device Number 1E9B
* Firmware…