Part Number: EVMASC-E99-B-50 Hello
I would like to get the design files of EVMASC-E99-B-50. I've got two eval boards and I need them
Could you help me, please?
thanks
Hi Ethan,
Thank you and I understand the condition for TCAN114x and TCAN1043A are different.
If possible, can you let us know what receiver timing symmetry is applicable for the following bit times (bitrates): 1) t_bit = 1/(1400*10 3 ) s (Bitrate…
Hi
we will share soon.
A query w.r.to issue
The battery pack is discharging to deep discharge level. But we have enabled PCHG Command( set value 1).But why the voltage is reducing and we could not charge the battery packs.
If the IC has 0V charging…
Part Number: BQ40Z50 Other Parts Discussed in Thread: BQSTUDIO The BMS never transitions to Sleep or Shutdown mode automatically, even though the system meets the required conditions (no load, no charger, no SMBus activity).
Current Configuration (from…
Oh and here is a full register read snapshot if it helps. I don't think there is anything obviously wrong in there but do please let me know if something isn't right! 1BAT_A_gg.gg.csv
Okay, I found the way to change BAL_EN bit (only charge mode can support balancing, right?)
but still CB bit = 0 with cell balancing start condition,
what should I do for it?
refer attached files check CB.gg.csv
Fullscreen
Check CB.log…
Hello Mitesh,
Thank you for reaching out to our team's E2E.
You can find the UL certificate for TPSI2072QDWQRQ1 on the UL website at the following link: FPPT2.E181974 - Nonoptical Isolating Devices - Component | UL Product iQ
For your convenience…
Hi Brian,
Attached is a document which covers what Texas Instruments devices have UL1577 certification as of 6-18-2024. The latest document can be found on the UL website.
In this document you can see the TPSI3052-Q1 covered.
UL1577.pdf
Best Regards…
Hi Venkatadri S, That help me understand the problem My motor max speed is 2500 RPM with 5 pole pair --> max speed is 208Hz I re-configure the CONST_PWR register with this value (208*16=3328) and now the motor behave as expected up-to 100% D.C. Thanks…