Part Number: EVMASC-E99-B-50 Hello
I would like to get the design files of EVMASC-E99-B-50. I've got two eval boards and I need them
Could you help me, please?
thanks
So it appears that both sensor 49 and 50 are sending temperature data, but the ZC is only observing reports from 49 in its application? And if you were to restart the test with commissioning sensor 50 instead of 49, would the ZC observe 50's temperature…
Hi Fabio,
There are two flavors of RMII: Master and Slave
Master
In Master Mode, the PHY operates off of a 25 MHz input clock.
PHY outputs a 50 MHz ref_clk that can be connected to the MAC
Slave
In slave mode, the PHY operates off of a 50 MHz input…
Hi Jeong,
Based on the register information you provided and assuming that the phase current shunt resistance (R44 on the MCF8329EVM) being used is 0.001mOhm We recommend changing the following current limits:
ILIMIT to 40%
LOCK_ILIMIT to 50%
HW_LOCK_ILIMIT…
Part Number: PROCESSOR-SDK-AM64X Other Parts Discussed in Thread: UNIFLASH Hello,
I have the eval board and trying to flash the sbl_null over uart. I could see letter 'C' displaying over COM6 and then disconnect the port , run the below command. It is…
Part Number: UCC28C43-Q1 UCC28C43QDRQ1's datasheet suggests that the RT resistance should be configured above 1kΩ.
However,we have using the RT/CT combination of 820R/1nF to produce a square wave with a duty cycle of 50% at 1MHz.
I hope to confirm…
I tried to compile Mobilenetv2 under tag 09_00_00_06 and set c7x_codegen to 1, but still couldn't run it
I only modified SDK_version and c7x_codegen in the script for compiling the model
The following is the runtime log, ”hhhhhhhhhhhhhhhhhhhhh“ is…
Michael and I get the same error message with the evm edgeai gallery examples running a freshly flashed 09.00.01.03 sd card image. If I click on any of the examples, nothing comes up and the following is printed out in the journal.
Apr 28 17:43:50 am62axx…
Hi Mark Fredette,
This app note explains these concepts in more detail: https://www.ti.com/lit/an/sbaa535/sbaa535.pdf?ts=1707854286390
Mark Fredette said: In AC or Chop modes the ODR is determined from the digital filter latency + the conversion delay.…
Part Number: MCF8316A Hi,
There days I am trying to run the MPET to get the MOTOR_R/L/BEMF CONST, there are something I could not understand.
The OL_ILIMIT_CONFIG was set to 0, the OL_ILIMIT was set to 8A, the faults of E2 was always 80080000, and always…