Part Number: EVMK2G Hi Experts,
Client is developing SBL on the EVMK2G board and stuck with some issues:
1. The board is not detected in CCS project wizard or TI DevTools. 2. Didn't find any guides on how to create CCS project for the board and project…
Part Number: EVMK2G I have been stuck on this for long. I am making changes to the loopback example provided for AUDK2G, the audio daughter card for K2G - I get my input audio input which is a 500Hz sine wave and store it in an int32_t array. I plot this…
Part Number: EVMK2G Hi experts,
For my work I developed a code on the evaluation board EVMK2G that is loaded in the DSP C66x .
I downloaded the ti-processor-sdk-rtos-k2g-evm-06.03.00.106-Windows-x86-Install.exe and I installed CCS10.2.
I developed a code…
Part Number: 66AK2G12 Hi,
processor - 66ak2g12.
IDE - CCS.
PDK - pdk_k2g_1_0_15.
i am trying to get a file from linux machine using FTP protocol for that i used example project of NIMU_FtpExample_evmK2G_armExampleproject from my examples, in the example…
Part Number: EVMK2G Hi experts,
For my work I am dealing with the porting of an application from OMAPL137 to EVMK2G. I state that I am new in DSPs; therefore, forgive me if my question is stupid.
I downloaded the ti-processor-sdk-rtos-k2g-evm-06.03.00.106…
Part Number: EVMK2G
Dear experts,
this post carries on my last thread in order to focus the subject on the last achievements
( e2e.ti.com/.../3984636
For my work I deal with the porting of an application for motor control from OMAP to EVMK2G by means of…
defconfig.zip Part Number: EVMK2G
Hi Ti forum!
I use linux sdk 06.03.00.106
I want to boot from QSPI flash and save env form/to QSPI. In uboot menuconfig i choise Environment is in SPI flash and see fails:
common/flash.c: In function ‘addr2info’:
common…
Part Number: 66AK2G12 Other Parts Discussed in Thread: OMAP-L138 Hello
I will use 66AK2G12 for the new project, so i'm testing it using the EVMK2G board.
I have experience in product development using OMAP-L138. When using the L138, i used the DSP…