Part Number: EVMK2H Tool/software: Code Composer Studio HI,
I try to burn the U-boot to EVMK2H with CCS on win10,but when I verify on UART, U-Boot show up nothing on the UART.
Here is my CCS version 7.3
U-boot file supply by processor sdk 06.01.00.08: …
Part Number: 66AK2H14 Hi,
I'd like to buy the EVMK2H or the EVMK2HX. However, it appears that the link for this EVM has been removed from the TI website. Has this become a not-for-sale item? If so, is there an alternative?
Best Regards, H.U
Part Number: EVMK2H Hi,
Recently, I use USB 3.0 hub connect to EVMK2H,so I could use more USB devices.
But I find out that when my USB device connect to USB hub , Linux will keep printing error message on Terminal
When I connect to EVMK2H directly without…
Sure thing,
Unfortunately I don't have the high speed scope on my hands anymore to see if there is still physical TX out of lane 2, but here is the register dump. Note that this is taken after LTSSM has finished.
Part Number: EVMK2H Hi all,
Do you have any workable example for the timer interrupt on EVMK2H ARM processor?
I try to modify the CSL example but cannot resolve "undefine reference" of function CSL_intcInit().
My project is as below:
ARM_Timer…
Part Number: EVMK2H Tool/software: Code Composer Studio SYS/BIOS 6.465.55, XDCtools 3.32.2.25 and GNU v4.9.3 (Linaro). Also, EDMA3 2.12.4, CTools 2.2.0, IPC 3.46.2.04 and Sys Analyzer 2.0.6.52? CCS 7.4.
My application has five projects; one on arm0 and…
Part Number: EVMK2H Hello everyone,
I have some querries about the EVMK2H Clock Frequency:
I read the register DEVSPEED (0x02620C98), the value is 0x00020000 , means the DSP is 1.2GHz and the ARM is 800MHz. Is it correct, as I thought the ARM core of EVMK2H…
Part Number: EVMK2H Hello
I'm working on Evm K2H
At the moment, I boot from flash using pre-built MLO, running RTOS on DSP0, and RTOS on ARM0;
I create 'app' file using 'out2rprc.exe' and 'MulticoreImageGen.exe'
MLO offset…
Part Number: 66AK2H14 Hi all,
I need to measure GPIO signal from EVMK2H board, what is suggested way to do so?
Thanks a lot.
P.S. I even purchase 120-pin connector, but it is too small to be soldered the wires to the pin.
Part Number: EVMK2H Tool/software: TI C/C++ Compiler Hello.
I'm newby in Embedded Linux.
I want to port network Linux application that includes <unistd.h>, <sys/socket.h>, <netdb.h>, <netinet.h>, <arpa/inet.h>, and so on. But when I try to compile…