Other Parts Discussed in Thread: UNIFLASH , SYSCONFIG Tool/software: Code Composer Studio
TI DevTools (dev.ti.com) will be down for maintenance from Fri July 31 20:00 to 23:59 EDT (Sat Aug. 1 00:00 to 03:59 UTC).
During this maintenance window, Resource…
Hi
Attached are the .txt files generated using my build environment
for CPU1 :
/cfs-file/__key/communityserver-discussions-components-files/171/flash_5F00_kernel_5F00_c28x_5F00_dual_5F00_ex1_5F00_c28x1.txt
for CPU2:
/cfs-file/__key/communityserver-discussions…
Hi,
PBMx is not a process designed for writing binary to EEPROM, it directly writes to device's SRAM.
When you are performing PBMx you do not need to write the full flash binary generated from the GUI as that is meant for EEPROM as there are two region…
Reg Data - Rx card register configuration:
00 h - 01
01 h - 70 (Initialisation) & 50 (Setup Rx)
04 h - 57
05 h - 48
06 h - 15
07 h - 5D
08 h - 57
09 h - 58
0A h - 15
0B h - 5D
0C h - 44
0D h - 54
0E h - E1
0F h - A3
10 h - 2F
11 h - E5
12 h - 57 …
Hi Craig,
I see. Can you please try flashing using the attached file instead along with Uniflash (available via TI.com). With this firmware, 4.1 will be MDC and 4.2 will be MDIO. In addition, it is recommended to powerup launchpad only when connected…
Hi Nicholas,
thanks a lot for the fast feedback.
So to understand from the post above is that you already have boards with the traces of LDO1 to the SD card domain of the SoC? To that affect, is the wrap wire populated and you're trying to avoid powering…
Hello Nicholas,
as suggested we pulled-up WD_DISABLE (GPIO8) to VCCA with a 10 kOhm resistor:
It seems like this made no change to the PMIC registers:
=> i2c md 12 0.1 0b 0000: 00 00 3c 7f 7f ff 02 0a 00 bf 00 ..<........
=> pmic dev pmic@48 dev…
Hi Glenn,
The previous attachment data is the data of port 360. Other ports may occasionally report some, but most of them are port 360. Customers can indeed provide register dump data of other ports at the same time, which I will provide in the attachment…
I'm trying to work with 9.0 for now.
github.com/.../r9.0
It installed as per the procedure.
./run_modelmaker.sh TDA4VM config_classification.yaml
When I train the model with the built-in config_classification, train says it's done, but I get an error…