Hi Adam,
I have try edgeai-tidl-tools master(09_01_06) without docker, it build io.bin and net.bin.
step.5, only onnx and 32bit result is different.
Because our model is training in BGR channel , I have tried different channel result
BRG_only_onnx …
This is what I see on the Capabilities section:
01:00.0 Unassigned class [ff00]: Texas Instruments Device b00d Control: I/O- Mem- BusMaster- SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx- Status: Cap+ 66MHz- UDF- FastB2B- ParErr…
I'm not aware of anything available for mating the Samtec 40pin connector with the 22pin FFC camera interface. The Samtec 40pin is design to interface with FPD-Link expansion boards like the Fusion design ( https://svtronics.com/portfolio/evm577pfusion…
Hi Jared,
I tried building the dtso file that enables the UART2 in SK-TDA4VM, please find the dtso file content below:
/dts-v1/; /plugin/;
#include <dt-bindings/gpio/gpio.h> #include "k3-pinctrl.h"
&main_pmx0 { main_uart2_pins_default…
Hello Gary,
Thanks for the above details.
A similar issue has already been resolved in another thread.
Please refer https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum…
Hello David,
you can modify an EVM (Rev. A+) to directly connect the RefClk pins from the AM64x to the PCIe slot. These are assembly options and you just need to resolder some 0 Ohm restistors.
You could look at the MCU+ SDK code to see how that configures…
Part Number: J721EXCPXEVM I have a J721EXCPXEVM , I am also checking J784S4XG01EVM.
I am looking for camera modules for these two boards, got a couple of questions during online search:
(1) Is the fusion board EVM577PFUSION-V1-0 compatible with both EVM…
Hi Seong-Il,
This thread solves a similar issue: https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/649818/ccs-tms320f28377s-product-c2000ware_software_package-v1-0-2-00-is-not-currently-installed…
Hello Krunal,
I tried this already before. For just being sure I tried again, the results did not change. You use "LP" version of am62xx. Could you try on the generic one (am62xx-evm)?
Here you can see the dts file and kmsprint results:
// SPDX…
No luck yet, but I updated the dtbo per https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tree/arch/arm64/boot/dts/ti/k3-am625-sk-mcspi-loopback.dtso?h=ti-linux-6.1.y
/dts-v1/;
/plugin/;
#include <dt-bindings/gpio/gpio.h>
#include "k3-pinctrl…