Part Number: EZ430-T2012 I need the connector part number for this board please .. i use the ez430 as a programmer tool and need to have the same mating connector as on the EZ430-T2012 part
Part Number: EZ430-F2013 The software on the disk will not install properly-missing files. Your web page, where this device is still being sold, has 404 failures for the software links. DigiKey also has stock of this device for sale. Please don't tell…
Other Parts Discussed in Thread: MSP430F2012 , MSP430F1122 , MSP430G2452
Due to the low pin count of launch pad i hav decided to connect a EZ430-T2012 - MSP430 USB Stick F2012 Board to launch pad via its ez430pin headers.
wht is the best way to keep the…
I have one of the new eZ430-RF2500 wireless development tool and I read somewhere that the old target boards (eZ430-T2012) are compatible with it (they originally work with the older eZ430-F2013 USB stick). I would like to buy some of the older target…
PERFECT! Assuming the statement "Supports eZ430-T2012 and eZ430-RF2500T target boards" is correct - and I have no reason to doubt it - this is exactly what I was looking for. Thank you!
TI says that "the eZ430-F2013 is a complete MSP430 development tool including all the hardware and software to evaluate the MSP430F2013 and develop a complete project in a convenient USB stick form factor." Which implies that the G2 LaunchPad with a DIP…
Just installed CCSv6 on a Windows 10 laptop, and it won't load code to a "T2012" card attached to an "ez430" programming demo tool,
reporting "Error Initializing Emulator: No USB FET was found."
The USB device was connected…
Ilmars said: You (conveniently) forgot what actually we are talking about: I didn't forget, but the discussion has somewhat shifted. However, back to original topic:
M. Joshi said: I may want to do some wireless interfacing later on.
I'd then go for…
Other Parts Discussed in Thread: MSP430F2012 Hi Friends, I have a small question and the case is as below.
I have MSP430F2012 with EZ430-T2012 Board
I have 2 motors connected through a motor driver which accepts pwm/dir input.
I have a joystick with 2…
Ian-- Thanks for the fast response again. I will pass this onto our assembly vendor and see what they say.
Is there any chance of TI offering the EVM target part as a product? We actually are using these in our prototypes. Kind of like the http://www.ti…