Part Number: F28M35M52C
Hello TI team,
We are maintaining a legacy F28M35M52C project in a regulated industry environment, using:
Code Composer Studio 9.0.1.00004
TI C2000 Compiler v6.0.2
We are trying to migrate from to compiler…
Part Number: F28M35M52C Tool/software: Hello,
I have a bootloader that downloads a flash image over CAN for programming into FLASH. The CSM is active with the following:
Z1 CSMPSWD set to password value
Z1 GRABSECT 0xFFF55555
Z1 GRABRAM 0xFFFFFFF5…
Part Number: F28M35M52C Other Parts Discussed in Thread: CONTROLSUITE , C2000WARE I cannot open ControlSuite From CCS resource explorer. Controlsuite version is 3.4.9. CCS version is 1120.
Part Number: F28M35M52C Hi Team,
Our customer would like to increase the pulse width of the EPWM of F28M35 microcontroller and would like to confirm if it is possible. Please see the details of his inquiry below.
I would like to ask you a question…
Part Number: F28M35M52C I have a customer with the following situation thanks for your help:
We want to add the firmware upgrade functionality for the device. We would need support from TI in order to use the Flash APIs.
Issue faced:
The module…
Part Number: F28M35M52C Hello,
We are using the Flash APIs in the F28M35M52C Concerto controllers.
We have configured the settings to access the Sector B in the .cmd file.
The sector B stores information which is required during firmware upgrade…
Part Number: F28M35M52C After a redesign following pins are not used any more:
PH5_GPIO53 Pin 47
PH2_GPIO50 Pin 36
PH3_GPIO51 Pin 35
PJ1_GPIO57 Pin 62
ADC1INB0 Pin 117
ADC2INB0 Pin 136
For the above GPIOs the TRM is saying that default config…
Part Number: F28M35M52C Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I have some confusion about the value of the decoupling capacitors used for +1.8V internal regulator output pins. The section 8.9.1 "Analog Subsystem: Internal 1.8-V VREG",…
Part Number: F28M35M52C i have 10 boards that contain concerto and tiva.
i used up to now the XF28M35h52 and the LX4F232H and all board were working.
i upgraded the boards to F28M35h52 and TMC123G .
5 boards are working fine and 5 boards faulty…
It looks like that update is failing because it can't find another update that the selected one is dependent on. What version of CCS is that? The versions of the components mentioned look pretty old as compared to the one I have. Plus win32 is mentioned…