Part Number: FDC1004 Dear Sir/Ms.
My customer is testing the FDC1004 EVM and found to be disturbed by radio waves. Some questions want to ask TI to help answer. (1) For the SENSOR distance, what is the material limit of the LAYOUT of the soft board…
Part Number: FDC1004EVM Other Parts Discussed in Thread: FDC1004 Dear Sir/Madam,
How many custom sensor can I connected to FdC1004evm?
There is only 2 shield connection, that means I can only connect to two copper sensor? Because the one copper sensor…
Part Number: FDC1004EVM Other Parts Discussed in Thread: FDC1004 , FDC2214 Hi Sir,
https://www.youtube.com/watch?v=Jtc15XAgXqg
This is the sample video from TI. Still thinking how to determine its sensing range.
It says that the sensing range…
Hi Kristin,
I am not sure if you can get this
email. I like to send you a few screenshots, but I did not find
any way to upload a file at the forum.
I saw it both on the Configuration tab
and on the data streaming tab as I logged…
Part Number: FDC1004EVM Other Parts Discussed in Thread: FDC1004 FDC1004EVM,With customer plate test(the plates are tiny, about the size of a fingernail), the chip output fluctuates greatly in the desired detection distance, and the useful signals are…
Part Number: FDC2214EVM Other Parts Discussed in Thread: FDC1004EVM , , FDC2114 , FDC1004 , FDC2214 Hello,
I am using fdc1004evm and fdc2214evm for distance measurements and wanted to double check if I'm doing it correctly, since I have some noise issues…
Yes, the TDC family can be used for liquid level sensing as well, and the signal strength will be strongest when the fluid surface is perpendicular to the ultrasonic sensor.
If you want more help with that solution, please start a new thread so that…
Part Number: FDC1004EVM Hi,
from the user guide i understand that after the gui installation the driver wizard is supposed to appear. unfortunately, it didnt, and my sensor is not being recognized.
What should i do?
best,
Dan
Part Number: FDC1004EVM Other Parts Discussed in Thread: FDC1004 What is the actual material used as shield and reference, level sensor.
And also, not able to download the firmware and gui from the TI link. Can anyone help