Part Number: FDC1004QEVM Other Parts Discussed in Thread: FDC1004 , Hi There,
I am trying to detect the liquid using the FDC100QEVM. As per reference designs, you guys are using more than one channels so I just wanted to know if it would be feasible with…
Part Number: FDC1004QEVM Other Parts Discussed in Thread: FDC1004 , FDC1004EVM Hello,
I want to write my own PC program instead use the TI program "Sensing Solutions EVM GUI". I can get the channel values via comport with the command "1". It is also possible…
Part Number: FDC1004QEVM Hello,
I have a question. If I read the register via i2c with Raspberry Pi 4, than I get the Information
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef 00: 03 20 02 19 01 31 01 85 10 3c 5c 7c 0d 00 00 00 ? ?…
Part Number: FDC1004QEVM Other Parts Discussed in Thread: FDC1004 Hi Ti Support Team,
My name is Xinghao. I am a graduate student from the University of Southern California. I am currently using the FDC1004QEVM board to measure multiple capacitive strain…
Chad, We don't have any history to share on the relationship between the tank material and the liquid to be measured. The material properties of the tank and the liquid are outside of our areas of expertise, and detailed information & guidance doesn…
Part Number: FDC1004QEVM Other Parts Discussed in Thread: FDC1004 Hi,
I use FDC1004QEVM with Sensing Solutions EVM GUI V1.10.0 to test liquid level.
Because my container is only 35 mm, the level changes is little.
I set the GAIN value to 3, and the…
Part Number: FDC1004QEVM Other Parts Discussed in Thread: FDC1004 Hi,
I am currently evaluating FDC1004 using FDC1004QEVM for liquid level sensing. I have a few questions related to FDC1004 but before going to the questions, here is a little background…
Part Number: FDC1004QEVM Other Parts Discussed in Thread: FDC1004EVM Hello, I'm trying to communicate the FDC1004EVM with Labview, but this software doesn't seems to detect the EVM. Do I need to install drivers or something like that? Thanks in…
Part Number: FDC1004QEVM Other Parts Discussed in Thread: FDC1004 Hi,
I have a problem with the FDC1004QEVM.
When i use completly the FDC1004QEVM with a stm32, all is OK.
But, when i cut the "usb to I2c part" and i add a 5K pull up, the fdc1004 don't work…