Part Number: FDC2212 Tool/software: Hi TI Experter,
Now, I am trying the shutdown function of FDC2212. I am using the pin of M03519 to control the SD pin of FDC2212. When the SD pin was high, I found that FDC was shutdowned. But, when the SD pin is…
Part Number: FDC2212 Tool/software: Hi Experter,
I am using FDC to detect the proximity. I met some issues. Can you help them?
My sensor is cylindrical copper foil. And it is connected to IN0A. The issues are describled as the lists
When the…
Part Number: FDC2212 Other Parts Discussed in Thread: FDC1004 Tool/software: Hello everyone, I am attempting to use the FDC2212 to measure the capacitance drift of a number of SMD capacitors as they undergo various environmental temperature/pressure,…
Part Number: FDC2212 Tool/software: Hi TI Experter,
I am using FDC2212 to design my proximity application. I would like to add active shielding to reduce signal interference. I am using the reference from TI experter to design the shielding circuit…
Part Number: FDC2212 Tool/software: Hi Sir,
When the customer uses FDC2212, the signal input terminal is connected to the sample needle (metal needle), and the sample position is plastic, which will cause static electricity, which will cause FDC2212…
Part Number: FDC2212 Tool/software: Hi Experter,
I am trying to use two channels to measure the proximity sensor. Currently, the first channel can work. But, the second channel cannot work. Can you help this?
I list my configured parameters:
{RCOUNT_CH0…
Part Number: FDC2212-Q1 Other Parts Discussed in Thread: FDC2212 , FDC1004 , Hi,
in our application the sensor capacitor (shaded grey in the image below) is a cylindrical capacitor whose capacitance we would like to measure.
So both plates…
Part Number: FDC2212-Q1 Other Parts Discussed in Thread: FDC1004 Tool/software: Hi John,
about 3 months ago, you proposed the FDC1004 instead of the FDC2x1y with the following reasoning:
"Also, many customers have struggled to get to production…
Part Number: FDC2212 Tool/software: Hi Experter,
I set up a board by using MSPM0 and FDC 2212. I tried to use I2C to configure FDC 2212. But, the communication cannot be set up successfully. For I2C bus, I have another device. I can use I2C bus to read…