Part Number: FLAT-CLAMP-TVS-EVM Hi
Please can you provide the CE/EU Declaration of Conformity for FLAT-CLAMP-TVS-EVM?
I could not find this on T.I website.
Thank you in advance
Part Number: LMX2592EVM Other Parts Discussed in Thread: LMX2592
According to the datasheet of LMX2592 Fig 6-12, the output power is nearly constant for all the frequencies.
But when we try to sweep across frequency with these settings, we are not able…
Part Number: TPS1HC100-Q1 Other Parts Discussed in Thread: TPS1HC30-Q1 , TPS272C45 Hello,
I am using a high-side driver (TPS1HC100-Q1) to drive an inductive load.
The single pulse turn-off energy for this high side driver is 35mJ.
But, energy stored in…
Part Number: FLAT-CLAMP-TVS-EVM Hello experts,
I have question about TVS series IC.
TVS series have some IN pin (Surge Protected Channel).
But layout example in datasheet shows that this IC protects one signal line. EVM schematic also show same case…
Part Number: TPS92520EVM-133 Hi team,
When I tested TPS92520-133 EVM, I found input VIN 0~25V, VBIAS is always 2V which is below the minimum input voltage(3V) of TPS7B8250. So the LDO didn't work.
After I shorted the D3, the LDO worked normally…
Part Number: TIOS101 Hi all
My customer is evaluating the TIOS101 and they have below questions.
Please review and comment.
Best regards
Ueli
---------------------------------
9.2.2.3 Driving Inductive Loads
The datasheet states: This voltage is clamped…
Part Number: SN65DSI86 Hi,
TI's EVM doesn't adopt any TVS in the eDP signal. We are curious of why eDP signals don't have TVS.
If eDP signal do need TVS, Do TI have any recommendation device?
Thanks.
Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
ESD Standards
Parameter Definition
Power Dissipation and Temperature
Top Threads
The following documents provide considerations…
Part Number: DRV8353RS-EVM Hello Team,
We would like to interface MAXON EC90 Flat Motor (Brushless DC Geared Motor) with DRV8353RS EVM. We are using Texas MCU which came default with this EVM (ISO-F2807F). We used DRV8353RS GUI to run the Motor, and…
Other Parts Discussed in Thread: TVS0500 Dear *,
i was going through SLVAE37
and have some questions regarding two calculations :
1)
"
The SMAJ33A has a RDYN of 884 mΩ, so a nominal VCLAMP = 38.6 V + (24 A × 0.884 Ω) = 59.8 V. This is…