Hello,
Oscar Gomez Fuente said: These two cases are the same, therefore we have the suspicion that they are wrong, but we don't know they have to be changed.
I would like to understand why for example afe2MaxDACCH1 is placed after the case 0x02 . I need…
Part Number: MSP430FR5986 Other Parts Discussed in Thread: MSP430FR6989 Hi all,
I'm developing my application on EVM430FR6989 of 100 pins, and I'm almost done with it and runs well (started with the base generated by FLOW ESI GUI). The thing is that on…
Part Number: MSP430FR5989 Hi everyone,
I am using the FlowESI GUI to generate my skeleton, but I think I have found another error. I would like to check with some expert to confirm me that.
My system is set to work with a maximum rotation frequency of…
Hi Dennis and David,
I've already had that suggestions in the code (FLOWESI GUI generates it), but nothing works. I wanted to start from 0 and I'm checking the examples of the workshop: lab_07b_lpm_timer_solution_msp430fr6989 --> Power consumption…
Part Number: MSP430FR5989
Dear TI team,
I have given to my customer a PCB using MSP430FR5989 for water metter with ESI and FlowESI GUI. The test are running well so they're pointing at the industrialization protocol, but there are a few things they…
Part Number: EVM430-FR6989 Other Parts Discussed in Thread: MSP430FR6989 , MSP-FET , MSP-EXP430F5529LP
Dear MSP team,
My customer is having a connectivity problem making use of the EVM430-FR6989. He has the CCS IDE installed to program the board together…
Also, the code that I use was generated with FLOWESI GUI, and that used SMCLK=2MHz, since I use SMCLK=8MHz, I changed a few things:
in ESI_TSM_INITPARAMS_DEFAULT structure, I changed ESI_TSM_SMCLK_DIV_1 to ESI_TSM_SMCLK_DIV_4
I added 2 extra lines in esiConfig…
Dear Cash Hao,
sorry for the late response.
That example code is not working for me.
In targetConfigs folder, there is MSP430FR6989.ccxml file. This file contains this code:
<?xml version="1.0" encoding="UTF-8" standalone="no"?>…
I'm not asking how to migrate the code for the CC1350 to the MSP430FR6989. I'm asking about the FLOWESI GUI software recomenden in www.ti.com/.../tidm-lc-watermtr , I'm trying to make it work wit the MSP430FR6989 Launchpad ( www.ti.com/..…
Part Number: MSP430FR5989 Other Parts Discussed in Thread: FLOWESI-GUI , EVM430-FR6989
Hi All,
I am developing a metering application which requires ESI sensing. I have adapted my code from FlowESI-GUI generate code program. As per the flow of the code…