Part Number: FUSION_DIGITAL_POWER_DESIGNER Hi Team,
We are using USB Interface Adaptor Texas Instruments 2022 Debugger & TI-Fusion-Digital-Power-Designer-7.8.3 software. & We are not getting any response. Kindly Check mentioned below Snapshot and help…
Part Number: FUSION_DIGITAL_POWER_DESIGNER Hello,
I developed a project in TI Fusion 7.6.1 and saved this as an XML file. I upgrade to Fusion 7.7.1 and try to import the XML project file, and get the following warning:
Please could you explain the meaning…
Part Number: FUSION_DIGITAL_POWER_DESIGNER I seem to be having some problems in TI Fusion design both 7.7.1 and 7.7.8 (Beta) when configuringthe LGPO of the UCD90320
I configure an AND path #1 and NAND path #2 into an AND gate: Configuring AND path #1…
Part Number: TPS536C7 Hi,
I'm using TPS536C7 multiphase PWM controller. Using the loop compensation parameters as shown in the below image, I'm getting around 22° phase margin. Please suggest on how should I change these parameters to achieve…
Part Number: FUSION_DIGITAL_POWER_DESIGNER I am using the Fusion Power designer to load code into a UCD90124A via the USB-to-GPIO adapter. I am using the .hex file format. Code loads correctly, but after the load I have to disconnect the USB-to-GPIO adapter…
Part Number: FUSION_DIGITAL_POWER_DESIGNER Hello, I have a tifsp file and would like to get the power sequencing chart from it in offline mode. What is the best way to accomplish this? Thanks in advance.
Part Number: FUSION_DIGITAL_POWER_DESIGNER Hello,
I am using the Fusion Digital power Designer application, along with part UCD90120 Aaddressed to 101d and 102d. When I run the application and change the control line usb from low to high which allows…
Part Number: FUSION_DIGITAL_POWER_DESIGNER I plan to use fusion digital power designer + the USB Adapter to program UCD9222 device.
Could the tool support command line ?Any guidance or reference can be provided?