Part Number: LM5160 Other Parts Discussed in Thread: TPS40170 I'm considering the LM5160 for a Fly-Buck, but the power requirements are on the high side (10-12W), according to the various app notes and E2E posts I've read. Could you recommend a Buck controller…
Part Number: LM76002 Other Parts Discussed in Thread: TPS62110 , Hi
Can I use TPS62110 or LM7600 using Fly-Buck topology the followung condition?
Vin=12V or 50V
Vout=±15V
Iout=300mA/ch
Frequency synchronization
Best regards,
Yok…
Part Number: LM5161 Other Parts Discussed in Thread: ISO5852S , Hiii,
I am designing a SIC Mosfet gate driver & gate drive power supply. I have selected ISO5852s as a driver. Below are the power supply specifications
Input voltage = 15VDC ( fully…
Part Number: LM5164 Tool/software: WEBENCH® Design Tools 1. I'm planning to get split rail (+/-19V at 0.4A each) from a single positive supply (+40V). The ground should be common to both input and output. I wonder if the following concept will work: …
Hi Robbie, One option is to connect the primary side as an inverting buck-boost to get a regulated -24.5V output. Then use a 1 : 1 turns ratio transformer to get an isolated 24V output. You can use the Fly-Buck quickstart calculator available online to…
Part Number: LM5160 Hi Team,
My customer used LM5160 as fly-buck controller, and reported several issues for startup/overcurrent/Cbst drop down issue.
The system setting is list as blow:
-- Input range: 15~18V[typical 16.5V];
--Primary output…
Part Number: LM5161-Q1
Hi,
We got a question from the customer about LM5161-Q1. Could you help us?
[Question] They evaluated LM5161-Q1 in Fly-buck-boost topology on their own board. Before the IC starts switching in start-up, the negative voltage…
Other Parts Discussed in Thread: LM5160A , PMP10733 , LM5160 Hi all. My customer would like to use LM5160A as Fly-buck. I sent Fly-buck user's guide of LM5160A to my customer. I would like to get reference Fly-buck layout, Please give me it.
Sorry I…
Hi,
As you know,fly-buck is a popular application in our design.
In this case,there are some questions to consulting:
1.What‘s the princilpe of this converter? Would you please explain it detaily?
2.What converters can used as a fly-buck? Only…
Part Number: TLV62568 Other Parts Discussed in Thread: TPS55010 hi team,
My customer is wondering if TLV62568 can be used as Fly-buck topology? Spec is 5Vin, isolated 5V out/200mA;
Thanks ahead for the support!
Regards,
Patrick