Part Number: INA118 Good morning,
I just wanted to check what is the platting of P/N INA118U or P/N INA118U/2K5.
In the datasheet, it states the following: Call TI | NIPDAU.
If we order one of these P/Ns, are we going to receive always NiPdAu?
I know that…
Part Number: INA118 Other Parts Discussed in Thread: INA188 , PGA308 , PGA309 Hi,
we are using the INA118 for amplification of a strain gauge force sensor. The unloaded sensor output voltage can vary between +64mV to -64mV due to tolerances of sensor and…
Part Number: INA118 Hello ...Are INA118U and INA118UB coming from the same die?
if yes then I can assume the wafer is screened and each element is sorted out for either INA118U or INA118UB
or if INA118U and INA118UB are not sharing same device then we…
Part Number: INA118 Per this E2E post here , the only difference between the INA118U and INA118UB is the box size. However, the specs are different in the electrical characteristics table. Can you confirm they're the same?
Part Number: INA118
In the past two years, components are very scarce, so we often can't get materials from TI's agent Arrow.
However, materials can be purchased from other channels, but they often paint labels. What's the reason?
For example…
Part Number: INA118
Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
" I want to amplify the RF signal with 50hz frequency and 400uv amplitude by using INA118 instrumentation amplifier, which will be fed with +-12vdc, by making…
Part Number: INA118 I am using an INA118 in a simple transducer application. The transducer is a Wheatstone bridge type sensor running at 10V. The INA118 is running single supply mode at 12V and the gain is set to 50 with a 1.02K resistor.
I have installed…