Part Number: INA132
Hi Team,
Good day! We wanted to clarify the input impedance in INA132. We need a clarification on the datasheet value of input impedance of INA132. The datasheet shows common mode and diff mode as 80k ohm whereas we understand…
Part Number: INA132 Other Parts Discussed in Thread: OPA2191 , INA826 , INA126 Hi Team,
The customer would like to use the op amp to design his circuit. The input signal is 0~20mV and it is 100HZ.
After the signal is amplified by the op amp, the output voltage…
Part Number: INA132 Attempting to mount an INA132A and puzzled at the lack of a clear pin 1 index mark.
There's no notch in the package. That circle within a circle is assumed to be locating pin 1 but it's not quite adjacent.
I'm going by that…
Shreeneet,
To achieve 36V common mode range you will either need need a higher supply voltage, or a diff-amp similar to the INA148 or INA149. I don't think you want to consider instrumentation amplifiers for this application as they generally have…
Other Parts Discussed in Thread: INA132 , TINA-TI In the INA132 spec, it says "do not interchange pins 1 and 3 or pins 2 and 5..." How should I interpret this? Can I rely on R1 and R2 to give me a gain very close to -1? Can I tie pins 1 and 3…
Other Parts Discussed in Thread: INA132 A customer is asking the following question about the INA132.
Can you get me data on long term gain drift of the INA132? Not pass/fail test data but real measurements? I need to estimate system 1 year accuracy…
Ok, input CM rejection sim with +/-0.1% on the Rg R's, need to add that in the opposite sense to the Rf as well, abou 55dB reject midband.
Now keep in mind the INA CMRR is freqeuncy dependent, So the INA132 suggested earlier looks like this over…