Part Number: INA163 Hi there,
Please could you inform me about terminal finish of the parts INA163UA / INA163UAE4 / INA163UA/2K5 / INA163UA/2K5E4. Could you tell me the thickness of Au in case the terminal finish is NiPdAu or NiAu or Au.
Thanks.
Best…
Hi Barry,
Here are the results from our thermal team for the SOIC package.
Theta JA 70 degC/W
Theta JC, top 25.8 degC/W
Theta JB 26.8 degC/W
Psi JT 2.6 degC/W
Psi JB 26.4 degC/W
Theta JC bottom N/A
Best Regards,
Chris Featherstone
Part Number: INA163 Hello!
I am attempting to use an INA163 for the first stage of an electroencephalography (EEG) tool. For that purpose, this is the design I was able to come up with:
My problem: whenever I plug the power supply, the amplifier starts…
Part Number: INA163 Other Parts Discussed in Thread: TINA-TI I'm working up a design using the INA163 for a microphone preamp but I also want to include the option of an unbalanced input. What is the preferred method to do this? Thanks.
Part Number: INA163 Other Parts Discussed in Thread: OPA1632 , , PCM4220
Hello,
I want to use the PCM4220 as the ADC. The ADC should be used to gather data from an condensator microphone. Also a turntable should be interfaceable. So the INA163 should…
Part Number: INA163 Other Parts Discussed in Thread: TINA-TI Hai,
I have developed a six channel mixer circuit, I got an small issue in this, I need a high gain and low noise op-amp , i have selected INA163 ic as a pre-amplifier. Can any one provide me…
Hi Steve,
Since the instrumentation amplifier is configured with a high gain of 2000V/V in this application, the noise of the instrumentation amplifier input stage will dominate and define the noise performance of the circuit. The noise performance of…
Part Number: INA163 I'm trying to amplify the voltage across a current sense resistor in-line with mains voltage. My INA163 is referenced to a separate ground, isolated from the incoming earth ground. I'm getting no output from the INA163. I have…
Hi Henrik,
Henrik Rosenø said: Doesn't TI have something like that, for frequencies at least in the audio range - possibly also higher?
Below is the selection of instrumentation amplifier. The list consists 2 and 3 -op amp instrumentation amplifiers…
Other Parts Discussed in Thread: INA163 , TINA-TI Hello, I am building an analog signal conditioning board for which the front end is the INA163, I am trying to create a "shelf-filter" type of response with a 22 nF in series with a 680 Ohm resistor, with…