Part Number: LP8864-Q1 Other Parts Discussed in Thread: INA194 Hi,
we have a LED PCB need to driver and the detail shown as blow
LED current: 220mA (max) LED counts: 38pcs
our LED Driver concept
my questions
any proposal for the LED driver select?
…
Part Number: INA194A-Q1 Other Parts Discussed in Thread: INA194 the output of INA194AIDBVT error and its up to 3.3v, the power supply of INA194 is 3.3V.
in our designer, the sensor resistor is 50mR.
Only one abnormal chip has been found so far, so can you…
Part Number: INA194 Other Parts Discussed in Thread: INA281 , Hello team,
Customer is evaluating INA281 as a replacement for INA194.
According to customer: We have an issue with this component where we don’t have any voltage on the pin Out.
Could…
Other Parts Discussed in Thread: LMP8640 , INA194 , INA281 Hi,
We need an alternative part for the nil-stocked INA914AIDBVR...please could you suggest one? We see the LMP8640, and wonder how that differs from INA914?
(We note the extra leg, but its NC so…
Part Number: INA194 Hi, We use the component INA194. The current can display from 200μA to 600μA depending on the component with the same electrical parameters.
Do you have an explanation for this problem? (Vin = 4.2V) Thanks Christian M
Part Number: INA194 Hi Support team experts,
My customer has a question regarding the power-up sequence regarding INA194. If supply of INA194 was established much slower than the input signals, will it cause damage on INA194. E.g. The +12V bus voltage…
Part Number: SN74LVC1G175 Other Parts Discussed in Thread: INA194
[Case:711493]Technical Data Inquiry for our customer.
1- Regarding each of the following parts:
TPS3808G01DBVTG LM5050MK-1 SN74LVC1G175DCK
-- Please help us know if each part is affected by…
Part Number: INA194 1. What is the maximum voltage on the IN+ and IN-?
2. When V+ is 0V, the voltage of IN+ and IN- is 60V, what is the maximum current that flows into IN+ and IN-?
Please advise.