Hello Guang,
I made some measurement with different value of power with my dynamic load (from 0A to 0.8A) linearity is good and amplification stage seems ok.
I "just" have a strong difference and i suppose i have an issue on my PCB because i have a 3mohm…
Part Number: INA215 Hi
Equipment using INA215 limits current to PWM. Distortion occurs in the INA215 output when the PWM frequency is 10 kHz or more. Is there a way to remove the distortion? Or please recommend a product that is available.
Thanks
Part Number: INA215 Hi all,
My customer have a question as the subject above.
What is the difference between INA215 A IDCKR and INA215 C IDCKR?
INA215 C IDCKR is little more expensive than INA215 A IDCKR.
Is it okay to use INA215 A IDCKR? they are very sensitive…
Part Number: INA215 Other Parts Discussed in Thread: UCD3138 Hello,
My customer is using the INA215AIDCKR device and they have reported that the output of the device oscillates when the PCB temperature reaches about 90C.
Please see waveform and partial…
Part Number: INA215 customer would like to bake their INA215 inventory them self. they would like to check TI's bake Conditions for Drying SMD’s at the INA215.
Can we have the bake condition for customer's reference.
I have an alternate proposal for you that might simplify this: would your team be willing to provide me with a design to perform current limiting during inrush using a current-sense amplifier (perhaps the INA215?) and op-amp on the feedback pin? We would…
Part Number: INA215 Hi.
INA215 DCK package is in use. I would like to know the criteria that judge a junction to be destroyed when the case temperature of the INA215 reaches a certain level. I find it very difficult to calculate using the formula provided…
Part Number: INA851 Other Parts Discussed in Thread: INA215 Hi,
can you please recommend a alternate part for the part "INA851" with singly supply 5V range.
Hello WJ,
Thanks for the question and using the E2E forum!
In general yes, to repeat what Clemens stated, lower input offset voltage is typically better as it introduces less error into your system and result in more accurate measurements. But as to which…
Other Parts Discussed in Thread: INA215 Hello,
I am looking looking at the TI high side current sense opamp, ina215:
http://www.ti.com/lit/ds/symlink/ina215.pdf
I don't really understand the purpose of the REF pin, could you please give me an explination…