Part Number: INA233 Hello, I have a strange problem with a custom board and a INA233 power monitor. I have eleven monitors on my board and the only one I've a problem with is address h4A. I'm only missing the first 2 bytes when I do a read from the device…
Part Number: INA233 Can you tell me the size and type of the volatile memory in the INA233?
Also, is there any non-volatile memory in the INA233? If so, what is the size and type of the non-volatile memory?
Part Number: INA233
I'm using a INA233 from an INA233EVM Kit.
I connected the board to a Mikrocontroller (nRF9160) via I2C.
The chip runs at 3.3V and monitors the power supply of the nRF9160 (VBUS also 3.3V, shunt 100mOhm, I between 25µA and 200mA…
Part Number: INA233 Other Parts Discussed in Thread: ISO1541
Hello, I'm using the INA233 to monitor a -20V rail and a -28V rail. I'm using the INA266 -48V Reference Design:
https://www.ti.com/tool/TIDA-00313
Here is how I have wired up the…
Part Number: INA233 Hi the customer is not familiar with our digital current sensor.
Whether we have the material about Configuration/Calibration Guideline?
Part Number: INA233 Hi,
My customer is looking for negative voltage version of INA233. Could you please let us know the right devices?
Negative voltage range is -20V to 0V. Please support us.
Thanks and best regards, M.HATTORI.
Part Number: INA233 Hi team,
My customer want to know what is the voltage sampling accuracy of IN+,IN- and Vbus?
What is the current sampling accuracy if they use a 3mR Rsense?
Part Number: INA233 Hello,
So I am having i2c issues linked to the INA233 where once we enable a brake motor the i2c communication fails. After some investigating we commented out getting the power value from the INA233 in our code. We are able to read…