Part Number: INA271-HT Good morning,
We are using your current amplifier INA271-HT, which has maximum operating temperature and storage temperature of 210C.
I was wondering if these are extended if it is supplied as unpackaged die (KGD for what I understood…
Part Number: INA271 Other Parts Discussed in Thread: INA281 Hello guys,
One of my customers is evaluating INA271 on their own PCB for their new products.
They compared two INA271 output voltage on same PCB when the differential voltage between IN+ and…
Part Number: INA271 Hello Guys,
Good day.
Our customer have some clarification on INA271. if he don't provide power to it, can he apply 60V common mode voltage to its inputs?
Thanks to confirm.
Art
Part Number: INA271 Other Parts Discussed in Thread: TIDA-00120 , TINA-TI Dear Specialists,
My customer is considering input low pass filter by adding capacitor between IN+ and IN-.
Resistance is device inside 5kohm.
Is it possible to use this method.
…
Part Number: PGA305EVM-034 Other Parts Discussed in Thread: PGA305 , INA271 , USB2ANY Dear, support team.
I have questions in circuitry around OWI in EVM.
No.1
This is OWI Block Diagram in datasheet (PGA305 EVM).
What are the functions of Offset Voltage…
Part Number: INA271 Hello guys,
One of our customers is evaluating INA271 now. Their evaluation circuit is almost same as the simplified schematic on page 1 in the device datasheet (SBOS381E). But one point is different from the schematic. it is that…
Part Number: INA271 Other Parts Discussed in Thread: INA282 , INA240 , LMP8645HV , Hi Team,
Do we have a pin-to-pin device with the INA271AIDR that has a higher gain, closer to 40V/V instead of 20V/V?
Thank you,
Jared
Part Number: INA271 Hello,
I used five INA271 circuits with 20 mOhm shunts on my board to sense current on five different voltage rails.
Two of the INA271 circuits are working fine. Three of them however, are not. Their are experiencing variable gain…