Hello Umar,
Assuming you are using the INA826 with a 510Ω shunt resistor as shown on the original post, with a gain of 97.86V/V:
The input stage offset is Vosi = 150µV (maximum) and the output stage offset voltage is Voso = 700 µV (maximum…
Hi Cyrille,
Cyrille Najean said: I wonder if TI can carry out temperature validation on a batch of components on request.
This is not part of our business. There may be a 3rd party service that is able to perform additional thermal and/or performance characterizations…
Part Number: INA826 Hello,
The datasheet states in the Characteristics table, that the Output offset is referred to input (RTI). so for the output offset, I would multiply the 200uV with the selected gain.
but in the formula, that is referenced by the…
Part Number: INA826S Hi Expert,
I do not understand how to understand figure 18. May I have your help to explain the relation for VCM.
Thank you.
Thank you.
Part Number: INA826 Other Parts Discussed in Thread: INA286 , Hi Everyone,
I am using INA826 for current measurement. Input SHUNT_A and SHUNT_B is connected to 100R resistor for current 0-10 mA. I have problem because when current circuit is open (current…
Part Number: INA826 There is a schematic diagram in which the +vs =24V ,-VS=Ref=0v, +IN < 24v , +IN > -IN >0v and G=1 as following:
Question: Is the equation true ?
Vout = G*(IN+ - IN- )
Thanks,
John
Part Number: INA826 Hi Team,
One question about the temperature drift of INA826. On this page what is the test condition? why the gain error drift is all negative in this diagram?
Also when Gain>1 will the temp drift highly related to the shunt resistor…
Part Number: INA826 Other Parts Discussed in Thread: TPS2661 , In this app note: https://www.ti.com/lit/an/sbaa551/sbaa551.pdf what is the purpose of R1 and R9 on page 3. Also what type of capacitor would be best for this application (such as C4)? I was…