Part Number: INSTASPIN-BLDC Hello
There is a project requirement for operating a Low inductance Very High Speed BLDC Motor.
Following are the specifications of BLDC motor: -
1. No Load Maximum Speed: 90,000 rpm
2. Number of Pole Pair: 1
3. Inductance…
Justin Walraven1 said: I will disable the PWM and spin in both directions and see what the Estimator does. Works?
The original lab can support the flying start that is disabled the PWM, but enable the FAST estimator always. You can check the estimator…
Andrea Mifsud said: #define USER_VOLTAGE_FILTER_POLE_Hz ((float32_t)(4000))
Filer pole seems high (4000) based on resistor divider network. What is your reference Hz set for motor ID?
Is the motor really capable of 100KRPM, seen a few on eBay are…
Part Number: INSTASPIN-BLDC Hello,
I am Integrating Modbus with the Instaspin lab now in c2000 there is three timer (0/1/2). My question here is Which timer i can use for Modbus application because in lab instruction was given that the
Timer 0: for frequency…
Part Number: INSTASPIN-BLDC
Hello,
I just searched and find out is not possible to use Insta-spin position control (LAB13B) without Index pin on encoder.
is there any way to have position control without index signal from encoder?
Thanks
Part Number: INSTASPIN-BLDC
Hi Team,
Our customer is looking for a library for speed estimation of brushed DC motor. Please see the details of his inquiry below. I've been using the INSTASPIN Lib for controlling a BLDC motor - which worked…
Part Number: INSTASPIN-BLDC Other Parts Discussed in Thread: MOTORWARE Greeting of the Day Dear,
I have my position setting follows
//Example: STPOSPLAN_addCfgState(handle, PosStep[MRev], PosStepFrac[MRev], StateTimer[ticks]); STPOSPLAN_addCfgState(stObj…
Part Number: INSTASPIN-BLDC Other Parts Discussed in Thread: LAUNCHXL-F280049C , BOOSTXL-DRV8320RS , C2000WARE Hi Team,
Our customer encountered an error while completing all the steps of InstaSPIN-FOC for F28004xC Lab Guide. According to our customer,
I…
Part Number: INSTASPIN-BLDC Other Parts Discussed in Thread: TMS320F28379D , TMDXIDDK379D , C2000WARE Hi,
We are designing a 10kW bidirectional inverter that is to drive a 30 V, 250 A, motor running at 135000rpm. Typically the input is 48V DC and it is…