Part Number: ISO224EVM Other Parts Discussed in Thread: ISO224 , , OPA2277 , OPA277 Hi Team,
My customer saw 500kHz 60mVp-p noise at output side(by differential probe to measure pin 6 and 7 of ISO224) during 0V input when they use ISO224EVM.
I saw this …
Part Number: ISO224EVM Hi team,
To confirm, which sample is installed on ISO224EVM, ISO224A or ISO224B? I would say the picture of the EVM shows the marking of ISO224B, but the schematic doesn't show the part number as specific A or B in the user guide…
Part Number: ISO224EVM Hello Experts, Do you have a layout pattern of the EVM? Customer would like to refer it for their layout. Best Regards, Fujiwara
Part Number: ISO224EVM Other Parts Discussed in Thread: ISO224 , OPA277 , AMC3330 Now I use iso224evm to test, the front-end uses 100A: 3.53v transformer to sample, and the signal is sampled to ADC through iso224 and opa277 amplification circuit;
连接如下:…
Part Number: ISO224EVM Other Parts Discussed in Thread: AMC1311 , AMC3330 Hi.
I'm trying to choose an evaluation module to test voltage sense for our application. I have some questions about my planned implementation.
In my application, I have a battery…
Part Number: ISO224EVM Other Parts Discussed in Thread: ISO224 To measure a 10V input to Vin do I need to provide 10V to VDD1 of ISO224 or can we use a 5V supply as given in EVM module
Part Number: ISO224EVM Other Parts Discussed in Thread: ISO224 , TLV6001 Tool/software: WEBENCH® Design Tools Hello,
I am designing isolated AC voltage sensing following ISO224EVM, In datasheet it is mentioned that VIN of ISO224 can not be more than 12…
Part Number: ISO224EVM Other Parts Discussed in Thread: ISO224 , TLV6001 Based off of the suggestion from a previous E2E post that I made, I'm implementing a differential to single-ended output conversion using TLV6001 like the one in the ISO224 EVM.…