Part Number: ISO35T Other Parts Discussed in Thread: ISO3086T Looking into using ISO3086TDWR to replace ISO35TDWR as a drop-in replacement to cover a shortage in supply.
I looked at the comparisons (link below) and we should be ok, but there are differences…
Part Number: ISO35T Other Parts Discussed in Thread: ISO3086T , ISOW1432 , ISO1500 , ISOW1412 , ISO1432 Hi,
Our customer is looking ISO35TDW for their end product. This part is out of stock. Is their other equivalent part in SOIC-16 package you can recommend…
Part Number: ISO35T How much accually Total current consumption require to VCC1 (also supply to T1 for VCC2) , 3.6V when design follow SLUU470?
from datasheet is specfiy 60 mA, 3.6V, and Typical efficiency 60% , that mean I have to supply 3.6V and 100mA…
Part Number: ISO35T I wonder if I use ISO35T to connect rs485 32 node vs 256 node, are they current consumption is it the same, 60mA for driver.
from datasheet is specify driver can take up to 60mA consumption.
Part Number: ISO35T Other Parts Discussed in Thread: PROFIBUS , ISO1176T , ISO1450 , , ISO35 Hi sir,
Whether that ISO35TDW supports profibus or not. I am sure that supports rs485 but we need to make sure to know about the profibus support of that chip.
profibus…
tens of MCUs have been replaced.
The thing is when I replace MCUs the problem always moves with the problematic part.
The interface device is TI ISO35T connected directly to the MCU UART.
I've the
MSP-TS430PN80USB - 80-pin Target Development Board…
Part Number: ISO35T Other Parts Discussed in Thread: ISO1430 , ISO1410 Hello
My customer is using ISO 35T in the following circuit. Primary Side is powered off. RS-485 side is active and 1.2VDC is applied to Y and Z. At this time, 0.5V is observed at the…
Hi Solarmax,
This reply is being posted for completeness to everyone following this thread:
Upon following up offline and testing on both Solarmax's end and TI's end, it was determined that the ISO35T devices used in this system were defective out of…
Part Number: ISO35T In the datasheet for ISO35T, one of the features states "Logic Inputs are 5V-Tolerant". However in the same datasheet the recommended operating conditions state that max supply voltage, Vcc is 3.6V and max voltage on logic inputs are…
Other Parts Discussed in Thread: ISO35T Hi,
My customer will use ISO35T.
If there is a transformer of recommendation, please tell me.
(Something of a surface mounting-type is desirable)
Best regards, itabi