Part Number: ISO5852SDWEVM-017 Other Parts Discussed in Thread: ISO5852S Hi, Good day. I hope you are doing well. Our customer is interested with the ISO5852SDWEVM-017 and they have an inquiry regarding this. Kindly see below: " We would like to know…
Part Number: ISO5852SDWEVM-017 Hi Team,
Our customer would like to know if the gate voltage of ISO5852SDWEVM-017 is programmable. I understand that the board measures 62mm like the standard IGBT but there is no hole for the terminal of the standard 62mm…
Part Number: ISO5852SDWEVM-017 Other Parts Discussed in Thread: ISO5852S , UCC21750 , ISO5852S-EP Hi Team,
We would like to driver CAS480M12HM3(SiC-MOSFET) by the circuit base on ISO5852SDWEVM-017.
Therefore, we have four questions.
[Q1]
If you have the…
Part Number: ISO5852SDWEVM-017 Other Parts Discussed in Thread: ISO5852S Tool/software: WEBENCH® Design Tools I try to find the design files to accelerate the design with ISO5852.
Part Number: ISO5852SDWEVM-017 Other Parts Discussed in Thread: UCC21750 Hi, I have the following query related to Half-bridge SiC eval boards: Do you provide power module boards (Power rating of 3-4 kW, and voltage of about 1 kV -SiC Mosfets) that can…
Part Number: ISO5852SDWEVM-017 Other Parts Discussed in Thread: ISO5852S
Hi,
I need better version of schematic. The file in the user guide is not so clear.
By the way, can we use one ISO5852 to drive two IGBT in parallel? Anything especially layout…
Part Number: ISO5852SDWEVM-017 Hello,
Is it possible to get a better version of the schematics in PDF format? The one in the User's Guide is very pixelated and hard to read.
Part Number: ISO5852SDWEVM-017 Hi,
In ISO5852SDWEVM-017, the isolated power for gate driver is generated through SN6505, in SN6505 datasheet, its output drive is only 5V 1A.
So I think the power generated can only be less than 5W?
But the source and sink…
Part Number: ISO5852SDWEVM-017 Hi,
in the TRM there is no data to show how it works with IGBT and MOS.
Like how long it has been tested with what current level IGBT, how's the thermal performance.
My customer would like us to offer such material. …