Part Number: ISO7731
Hi team,
My customer found a issue about ISO7731DWR, could you please help review and give some suggestions? Thank you.
The problem is the waveform on the output side OUTC(5pin) and the input side are inconsistent, with a large number…
Part Number: ISO7731-Q1 Other Parts Discussed in Thread: ISO7731 In the application I'm working on, I would like to enable the digital isolator using a soft start (RC) pin the controller on the primary side. For this I would be interested in the enable…
Part Number: ISO7731-Q1 Hello,
I would like to understand what copper isolation i need to have between pad to pad. The spec say that i can have 5KV isolation, but if i use the calculator: https://www.smps.us/pcbtracespacing.html with 5000V, it give me 572mils…
Part Number: ISO7731 Other Parts Discussed in Thread: ISO6731 , ISO7831 The creepage distances of ISO7731 and ISO6731 Only 8mm, it cannot meet customer demand that is 11.5mm creepage distances, so I would like to ask if there is an isolation plan that…
Part Number: ISO7731 Hi,
I am trying to use the circuit provided on the PDF entitled "Designing a reinforced isolated I2C bus interface by using digital isolators" but am unable to get it working. I have built the "Final isolator circuit" shown in fig…
Part Number: ISO7731-Q1 Hi,
I'd like to know how to calculate the maximum propagation delay for a digital isolator when using different supply voltages.
I'm presuming that the device is intended to be able to run with different voltages on the two…