Part Number: ISO7741-Q1 Tool/software: Hi team,
Please help review whether the power supply of ISO7741-Q1 is reasonable. If there is any need for improvement, please point it out.
The two schematics are two independent power supply methods and the…
Hi Hangjie,
Thanks for reaching out.
Hangjie Wang said: And if we use this device on 400V battery, whether the DBQ-16(300Vrms working voltage) suitable for the 400V BMS system?
In the insulation specifications from the datasheet, The Maximum…
Part Number: ISO7741-Q1 Other Parts Discussed in Thread: ISO7741 Hello together,
I want to use the ISO7741 for galvanic isolation of a SPI-Interface (and 2 other signals) When input and output are not connected this works well for my transfer rate of…
Part Number: ISO7741-Q1 Tool/software: A number of TI isolators have DIN EN IEC 60747-17 (VDE 0884-17) reinforced certifications. One of the major requirements of reinforced insulation in this standard is a 1ppm failure rate over lifetime [FROL] based…
Part Number: ISO7741-Q1 Tool/software: I was recently pointed to the DWW package version of the ISO7741-Q1, which has a 33% higher voltage rating than the DW package.
I've noted a number of oddities in the datasheet which lead me to questions:
Page…
Hi Matthias,
Thanks for reaching out.
Matthias Geipel said: What is the maximum output leakage current of a disabled output OUTx? Is it below 1µA, in the range of 10µA or is ist higher? I couldn't find this in the datasheet.
This is not specified…
Part Number: ISO7741-Q1 Tool/software: Hi,
I am using ISO7741FBDWR as isolated 1mbps UART. I found that communication is not being transferred to isolated side from MCU.I am attaching my schematics> Please let me know if there is any mistake
Thanks…
Part Number: ISO7741-Q1 Other Parts Discussed in Thread: ISO7740-Q1 , Tool/software: I noticed that ISO7741-Q1 and ISO7740-Q1 are getting a bunch of their Part Numbers discontinued. For example, ISO7741FQDBQQ1 is being replaced by ISO7741FQDBQRQ1.
The…
Part Number: ISO7741-Q1 Other Parts Discussed in Thread: ISO7741 , ISOW7741 hi expert
i saw this link Fundamentals of EMI Requirements for an Isolated DC/DC Converter (ti.com) . in this note, it show two solution to improve EMI: one is to add "Interlayer…