Part Number: ISO7760 Hello Team,
looking at below table I calculate a max frequency of 1/6ns = 167MHz which means a data rate of max 333Mbps should be possible.
Please let me know if my calculation is correct. My customer plans to use the ISO7760 at…
Part Number: ISO7760-Q1 Other Parts Discussed in Thread: TVS0500 , TPS25947 , Hi,
Please refer to attached drawing
I am designing a MCU board which will communicate with a daughter board to get sensor data.
Some data lines are connected between MCU and daughter…
Hi Rao-san
Thank you for your reply.
I understood the device has been sufficiently tested and verified.
My customer wants to have the proven data that the carrier frequency of ISO7760 is 450MHz.
EMI data of ISO7760 is also ok for him.
Best regards,
Shunsuke…
Part Number: ISO7760 Other Parts Discussed in Thread: ISO7763 HI
Could you help suggestion suitable devices can Replacement ADuM163N0BRZ
Thanks
ADuM160N/ADuM161N/ADuM162N/ADuM163N (Rev. A) (utmel.com)
Part Number: ISO7760 Hello TI experts,
I just saw the part name ISO7760F in ISO7760 datasheet.
but i cannot find any description in it.
what is the difference between these 2 devices?
Best regards,
Chase
Part Number: ISO7760 Hi, Good day. Is it possible to use a different supply for the primary and secondary side of the ISO7760 and similar digital isolators (e.g. 5V primary and 3,3V secondary)? Thank you. Regards, Cedrick
Part Number: ISO7760 Other Parts Discussed in Thread: ISO1212 , ISO1211 Hello Guys,
Good day.
Our customer is having troubles with the isolator ISO7760DBQR in the isolation test. They have a loop when the supply is off and there is a high level in any…