Part Number: ISO7761 Dear Sir or Madam,
my colleague and me used two different ways to determine the FIT rate for TI part number ISO7761DBQR.
My colleague scanned your technical documentation and used the functional safety information where the fit rate…
Part Number: ISO7761 Dear Sir or Madam,
Could you inform me about terminal finish of the part ISO7761FQDWRQ1. Could you tell me the thickness of Au in case the terminal finish is NiPdAu or NiAu or Au.
Could you provide me with ECCN (Export Control Classification…
Part Number: ISO7761 I am using ISO7761. The data sheet states the following, but I think the actual operation is different from the description. Attached is the circuit diagram and waveforms.
According to the data sheet, when VCCI is PD (<1.7V) and VCCO…
Part Number: ISO7761-Q1 Hi Expert,
My customer is facing shortage on ISO7761FQDBQRQ1. May you kindly check if we have P2P replacement for this device? No need to change the schematic/layout.
Thanks!
Ethan Wen
Part Number: ISO7761 Hi Team,
Good day! I am posting this to help our customer and find solution for their concern. Kindly help.
I am not sure whether IO denotes just the output current iof one channel or it is the total sum of all channels output…
Part Number: TMDSEMU110-U Other Parts Discussed in Thread: ISO7761 , TMS320F280049 Hello, customer want to isolate the JTAG with our ISO7761 but CCS often complains that the MCU is in Low-power mode… Error -1156)
Is there something what he has to…
Part Number: ISO7761-Q1
Hello,
We are using ISO7761FQDWQ1 digital isolator in our design.
I want to confirm below point:
In the ISO7761FQDWQ1 IC, 5 channel are forward and 1 is reverse, Considering this case:
Vcci/Vcc1 is the input power supply for…
Part Number: ISO7761 Hi, support team
My customer has the questions as follow:
Are there alternate parts for ISO7761FDW and AMC3302DWER?
Thanks so much.
Best regards, Yuki
Part Number: ISO7761 Hello,
I have a questions regarding the layout. Is it possible to place 2 of these ISO7761 back to back (top and bottom) on a 93mils thick PCB?
thank you,
-Long