Part Number: IWR1843BOOST Hi,
I succeeded to setup and connect the EVB IWR1843Boost with my PC with the TI dev cloud.
What is the right way to:
1. Set Real and Imaginary data for each Tx channel from the EVB?
2. Record into my PC the Real and Imaginary…
Part Number: IWR1843BOOST Hi,
I am trying to sync two AWR 1843 radars, following https://software-dl.ti.com/jacinto7/esd/robotics-sdk/08_05_00/docs/source/docs/multi_sensor_time_synchronization.html .
And i am doing the SW approach. but it given the following…
Part Number: IWR1843BOOST I'm facing a software crash issue with our radar system in the MRR lab. Here's the breakdown:
FPS Dependency: As discussed in this thread the radar's frame rate (FPS) depends on the SUBFRAME_MRR_PERIODICITY_VAL parameter…
Part Number: IWR1843BOOST Hi, thank you for the previous support.
I try to connect the EVB with the software "mmwave_studio_02_01_01_00_win32".
We have a problem connecting to the EVB, which connected to COM port 5:
I try to connect with thw…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: IWR1443BOOST Dear Sir
I received the following answer to my question.
This is already working with mmwave Demo Visualizer running in function mode.
What I would like to know is that I sent the…
Hi Josh,
I'm still looking at this too - and I've found something to report: indeed, something seemingly so strange, that it must be a pointer to what's going on.
In the "real" system, the IWR is synchronised with other h/w via GPIO_1 ..…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: IWR1843 , IWR6843 , IWRL6432 Hi,
I am Surya. I am working with IWR 1843 BOOST for vital signs detection. I have few questions and i need support in working with it.
1. Can IWR 1843 BOOST be used…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: DCA1000EVM Hi. I wish to acquire data from the 1843 BOOST and was wondering if you can provide everything I would need hardware wise. Ultimately I am seeking a quote for purchase. I see that the…
Part Number: IWR1843 Other Parts Discussed in Thread: DCA1000EVM Hi, TI support team
Hope this email finds you well.
I am writing because I have met some problems when I want to get raw data from mmwave studio.
my device is DCA1000EVM and IWR1843BOOT…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: IWR1843 , UNIFLASH Hi,
maybe hardware failure?
All working OK, developing & debugging in CCS 11 (update to 12 ... same error). Suddenly get this error:
Error connecting to the target: (Error…