Part Number: K2GICE Tool/software: Code Composer Studio Im trying to find example sources for the ethetCAT software delivered in sd card with the board. Is this available somewhere.
Other Parts Discussed in Thread: K2GICE , 66AK2G12 , TPS62180 Team,
A project was started based on the 66AK2G 02 ICE (K2GICE) board that has a discrete power tree: http://www.ti.com/product/66AK2G02/toolssoftware#desKits I assume the the latest K2GICE board…
Part Number: K2GICE Other Parts Discussed in Thread: 66AK2G12 Hi guys,
I am wondering why both K2G EVM and K2G ICE boards have pull up resistors for both QSPI_D2 and QSPI_D3 pins but not QSPI_D0 and QSPI_D1? Is it ok to add pull up for D0 and D1?
Thanks…
Hello Nick,
Thanks for the response.
I am not getting any bus error from the methods you suggested.
I seem to into segmentation fault when I access the memory that might be due a bad pointer or clean-up issues which I am yet to resolve.
I would…
Part Number: K2GICE Tool/software: Linux Hello,
I am trying to build the sdk on k2g-evm on Ubuntu 16.04 64 bit version using the steps mentioned in the below link:
http://processors.wiki.ti.com/index.php/Processor_SDK_Building_The_SDK
I have tried to…
Part Number: K2GICE Hi TI Experts,
Please let me confirm the following question.
[Question] Can K2G device support the EtherCAT Master? If yes, would you please teach me the schedule to provide the sample code?
Best regards. Kaka
Part Number: K2GICE
Tool/software: Code Composer Studio
hi all~
I'm testing the gigabit port of K2GICE in CCS v7, pdk k2g 1.0.8, ndk 2.26.0.8. (these are the latest version, I think)
Using pdkProjectCreate.bat file, examples are created.
import…
Part Number: EVMK2GX Other Parts Discussed in Thread: 66AK2G01 , K2GICE , 66AK2G02 , , 66AK2G12 How to build, run and test the EMAC example from TI-RTOS PDK for the K2G family processors (EVMK2G, EVMK2GX, EVMK2GX, 66AK2G01, 66AK2G02, 66AK2G12 and K2GICE)…