Part Number: LAUNCHCC3220MODASF Hello everyone,
Although the memory location starting at address 0 is not mentioned in the link command file of the application, some corresponding entries appear in the map file. 00000000 __ASM__ 00000001 xdc_rov_runtim…
Part Number: LAUNCHCC3220MODASF Other Parts Discussed in Thread: SYSCONFIG hi I am working with simplelink_cc32xx_sdk_4_10_00_07 and ccs version 12.0. Trying to setup a modbus (rs-485) code uart write function was successful but my code is stuck on uart…
Part Number: LAUNCHCC3220MODASF Hi,
We use external RTC ds3231 to get date and time. We are using default I2c library ti/drivers/I2C.c but while writing timing to DS3231 I experienced I2C transfer failed. If I connect DS3231 to esp32 it works.
Procedures…
Part Number: LAUNCHCC3220MODASF Hi,
We use rs485 modbus (max485) which is half duplex communication. How to set uart parameter? We use the UART parameter structure below
UART.c typedef struct { UART_Mode readMode; /*!< Mode for all read calls */ UART_Mode…
Hi,
As mentioned, you can go error by error and resolve manually but you can also use one of the existing projects that works and replace the existing source files with the ones from the plugin. It is required to do some manual integration but since the…
Part Number: LAUNCHCC3220MODASF hi, I am testing the mqtt_client_over_tls example code to publish a dummy message to our Azure cloud platform, for which I add "DigiCertAssuredIDRootG2.crt.pem" to the user file and change the global variables…
Part Number: LAUNCHCC3220MODASF Other Parts Discussed in Thread: CC3220SF Hello TI Community,
I have a query regarding the power management of CC3220MODASF. After reviewing the technical guide for CC3220, I found reference to a pre-regulated 1.85V alternating…
Part Number: LAUNCHCC3220MODASF Hello TI Community,
.
I am currently working on a project to integrate Modbus communication into a CC3220MODASF and transmit sensor data to Azure Cloud. I am using an SD card over spi protocol to store the sensor data and…
Part Number: LAUNCHCC3220MODASF Hi, Is it feasible to utilize the CC3220MODASF UART for both the Tiva MCU and independently through the 20-pin connector simultaneously? Our goal is to conduct testing and debugging of an external UART, so we need to use…