Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 After building Project for pwmled2_CC1310_LAUNCHXL_tirtos_gcc I am getting the below mentioned window, The target become connected but DI06 and DI07 Led don't active. How will I solve…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 , LAUNCHXL-CC1310: Whether CC1310 High Speed Mode has use PN9_WhiteDate to process message?
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 , Currently, I am using the LAUNCHXL-CC1310 development board (CC1310 Launchpad Rev: 1.4, CC1310F128RGZ) for red LED turns on, when a certain amount of time has passed (10 sec) and turns…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 , WMBUS I want to implement M-BUS using CC1310 transceiver's, and want to know the frames of M-BUS sent from the device side towards the collector.Also,the responses for the same. …
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: UNIFLASH I am trying to start a project using CC1310F128RGZ Microcontroller. After clicking verify, it appears an error mentioned below-
An error occurred while hard opening the controller. …
Part Number: CC1310 I have to configure CC1310 devices in a star network. The central device is a CC1310 that interacts with several CC1310 devices wirelessly. The address has been configured to be 8 bytes. Could someone please guide me on how to use the…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 Hello everyone. I am working with a SPI slave device. Which requires the host to send an 8 byte command and the slave responds with an IRQ for the host to issue two bytes of mode change…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 Hello everyone. I am working on the interconnection of a RFID module through the four-wire SPI interface (CLK,MOSI,MISO,SS). A CC1310 as master. The datasheet of my slave device specifies…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 Hi all.
I try to combine SPI Slave and RF Tx module.
I attached to SPI slave blocking mode in my code. It run but not correctly.
I want to work synchronize with SPI Master.
I want to…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 , UNIFLASH
Hi
We have a mix of 64KB and 128KB CC1310 devices and we need to be able to detect the device type and program the correct firmware in it accordingly. Using "Flash Programmer…