Part Number: LAUNCHXL-CC1312R1 Hi team,
Is it possible to receive the packets encoded by Manchester Encoding like the figure below? In customer's use case, competitor's sub1GHz module sends Manchester Encoded packets, and CC1312 receives it.
…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: CC1312R Hi TI team,
I was looking for a tool to read contents of external flash on CC1312R1 and R7 (flash - Macronix MX25R).
The only tool I could find was "flash-rover" ( https:…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: SYSCONFIG Hi team,
May I ask you questions regarding manchester coded binary modulation?
1. My customer would like to set the protocol to manchester coded binary modulation(FSK/GFSK). May…
Part Number: LAUNCHXL-CC1312R1 Hi team,
My customer would like to configure the RF frequency to 1200MHz, but it seems like CCS doesn't allow to do it from the figure below. Are there any ways to configure RF frequency to 1200MHz?
Best regards,
Shunsuke…
Part Number: LAUNCHXL-CC1312R1 Hey,
I use CC1312R1 and I've noticed that sometimes when i turn off the voltage supply, the FLASH erase itself.
I had some research and it occurs because the CS (Chip select) is trying to write while VCC is going down…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: UNIFLASH , , CC1310 , WMBUS , CC1350 Hi!
I'm trying to flash a launchxl-cc1312r1 with "Serial_CC13xx_Collector_T2.hex", so I can communicate with the device via the SATP API Interface. I have…
Part Number: LAUNCHXL-CC1312R1 Hi TI team, I have a general question about NVS implementation to read / write to external flash (Macronix MX25R)
What is the rule of thumb using NVS_open() and NVS_close().
For each read transaction should I call NVS_open…
Part Number: LAUNCHXL-CC1312R1 I have a project that I import that when I build shows: Product com.ti.SIMPLELINK_CC13XX_CC26XX_SDK v7.10.2.23 is not currently installed. I did install the SDK SimpleLink Low Power F2 SDK 7.10.02.23. Is this the correct…
Part Number: LAUNCHXL-CC1312R1 Hello,
I have two launchxl-cc1312r1 and try to download example tx and rx (project0) use CCS cloud ( dev.ti.com/.../node .
I have installed ti browser extension and ti cloud agent. But I get error for each module
1st module…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: WMBUS , , SYSCONFIG , CC1312R Hello, I want to develop WMbus communication using LAUNCHXL-CC1312R1 and a smartmeter that use 433MHz. but there is no WMBus option in sysCfg when I select 420 …