Hi Daisuke-san,
Daisuke Maeda said: Was a heatsink used for the AM62x on the board used for measurements in the application note?
There was not one used. Instead a Thermal Flow System, TFS.
Daisuke Maeda said: What is the airflow (m/s) under temperature…
Part Number: TMS320F280038C-Q1 Hi,
there is a power estimation tool available for F28004x -> https://www.ti.com/tool/C2000-F28004X-POWER-EST-CALC
Is there something available or planned for F28003x ?
Thanks and best regards,
Gregor
Part Number: ZIGBEE-POWER-CALC TI is pleased to announce a new TI Arm Clang Compiler Tools release 3.2.0.LTS which includes the following new features.
New features:
Support for ELF Segment "Blocking" (Alignment and Padding)
Support for OpTI…
Other Parts Discussed in Thread: ANALOG-ENGINEER-CALC I messaged TI and they said I should post here. Maybe with enough interest TI will update the ANALOG-ENGINEER-CALC tool. My suggestion is to allow entry of one of the calculated values. In the Passive…
Part Number: AFE7952 Hi,
I find out a good tool in TI; https://www.ti.com/tool/FREQ-DDC-FILTER-CALC
I set Fs=2900MHz, Interleave=1, Fc=2050MHz, BW=1MHz.
I get: Rx band=850MHz, HD2=1200MHz, HD3=350MHz, HD4=500MHz, HD5=1350MHz
"slyt738.pdf" The TI doc. show…
Part Number: AFE7952 Hi,
I find out a good tool in TI; https://www.ti.com/tool/FREQ-DDC-FILTER-CALC
I set on sheet-2 ; Fs=2900MHz, Interleave=2, Fc=2050MHz, BW=1MHz.
I get: Rx band=850MHz, HD2 image=250MHz, HD3 image=1100MHz, IL=600MHz
1: Interleace=2…
Part Number: AM62X-PET-CALC Other Parts Discussed in Thread: SYSCONFIG Hi TI
In the AM62x Sysconfig tool , i found there is only one volteage option can be select ,but in schematic design i assign two power rail for VDDA_1P8_USB/VDDA_3P3_USB, seems confict…
Part Number: AM62X-PET-CALC Hi TI
In the power estimation tool, how to selec the mode column list as below?what's the represent meaning of every item?when i used this port as GPIO which one can i select?
BR JINGCHENG