Part Number: LDC1101 Hello,
Hope you are well.
I've been using the LDC1000 for position sensing. Recently, I tested the LDC1101. I just wanted a quick confirmation on something.
On the LDC1000, when my sensor is closest to the target (lowest Rp),…
Part Number: LDC1000EVM Hi Team,
My Applications
Question 1: This is a four-pole magnetic bearing, and my purpose is to make the rotor in the middle stable suspension at all times during the bearing operation. A sensor is required to detect the position…
Part Number: TMS320F28379D Other Parts Discussed in Thread: LDC1000EVM , LDC1614 , LDC1101 , LDC3114
Hello everyone,
Up until recently, I was using sensors from the LDC1000EVM evaluation module. I snapped off the USB module from the EVM, and wired the different…
Part Number: LDC1000EVM Hi,
Best regards.
I would like to know if I can use the LDC1000 as an NCV sensor (Non-Contact Voltage). The idea is to determine if there is AC current passing through the transmission line
Thanks in advance.
Hi Kristin,
I performed another few comparison measurements to confirm that the LDC1101 performs better with higher sensor capacity.
First I used a self-wound copper coil together with a 1000pF capacitor. In this scenario the LDC1101 had a much better…
Part Number: LDC1000 Hello,
we see following effect when our magnetic Encoder ring starts turning. Can you explain this behaviour?
I expect same behaviour will occur when switching to the successor chip LDC1001?
Thanks in advance.
Regards
Frank
Part Number: LDC1000 Hi,
I've recently inherited a design based on the LDC1000. Two queries.
Readings of the proximity data registers are highly sensitive to temperature. I understand this is due to the inherent temp co of our PCB based sensor winding…
Clancy -
We are considering using the LDC1000 for a proximity sensor in a commercial application which has a 10 year support requirement. Please contact me to discuss product availability.
Thanks
Tim
Part Number: LDC1000 Greetings,
Just came across LDC sensors. Need to know if these can work in my use case or not.
I am working on a project where i want to know if there is an abnormality on the metal surface like a hump or crack. Hump can vary from…