Part Number: LDC1101 As part of existing project we are using LDC1101 and i am responsible for the HIL testing of the whole product.As per the requirement i need to have a plant model including LDC1101.could you able to provide a dummy matlab simulink…
Part Number: LDC1101 Tool/software: I have used the old online version of the LDC Design Tool in the past. Had no issues with it and was easy to use.
Using the new spreadsheet version:
For this project, I am considering the LDC1101. I downloaded the…
Part Number: LDC1101 Tool/software: Hello,
We are seeing our Rp/L measurements take longer than predicted by Formula 10 in Section 9.1.8 of the datasheet.
Our sensor frequency is 4 MHz.
Here are the values we measured experimentally, by using an…
Part Number: LDC1101 Hello, I am seeing Time Constant numbers from the LDC_Tools-ext51 spreadsheet that seem to be differing from the guideline given in the LDC1101 datasheet section 9.1.5, 9.1.6.
Constants used in the below calculations are as follows…
Part Number: LDC1101 Tool/software: Hello all,
I am using SPI on the 2800137 launchpad to communicate with a LDC1101.
If I use the SPI_transmitByte() function and pass the appropriate READ/WRITE command along with a register address of the LDC1101…
Part Number: LDC1101 Hello,
I would like to design a sensing coil for the LDC1101.
Which parts list in Coil Designer should I select? (See attached PNG File)
Thank you,
Tomo
Part Number: LDC1101 I have three LDC1101 chips in a space constrained design. To save space, I would like to connect the output of a clock source to the reference clock inputs of all four LDC1101 chips. Another forum post mentioned that the reference…
Part Number: LDC1101 Other Parts Discussed in Thread: LDC1001 , , , LDCCOILEVM , LDC1614 , LDC1612 , LDC1312 , LDC1000EVM Hi, I'm very confused. I need to sense a metal object about 20-30mm far from the sensor. And I have space constrains so the sensor…
Part Number: LDC1101 Hello,
I need to use the LDC1101 to sense the distance to a target. The LDC1101 will be 1 mm away from the target and the target can move 3 mm away from the sensor. I have tested the same setup with an aluminum target and the results…
Part Number: LDC1101 VDD is powered from 3.3V digital and ground and the Rp values are excessively noisy. Don't have the common mode filter laid out on the board, so I only have the two 0402 EMI caps on the INA/INB pins to ground to mitigate EMI susceptibility…