Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 Hey All.
Simple question.
The LDC1101 seems to have a maximum sampling frequency of 5.3uS, is this correct or am I reading it wrong ?
If correct or not, what settings ( sensors frequency…
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 , Hello im trying to use the ldc1101 evm gui, and it seems to be stuck in simulation mode. i can not change any settings other than the com port that it should be connected to. i have lab…
Part Number: LDC1101 Hello all I im working with the ldc1101evm board and my own board with the ldc1101 chip. as of now they have basically the same layout, but the ldc1101evm gives a constant value of about 47k counts with a std dev. of about 100 counts…
Part Number: LDC1101 Other Parts Discussed in Thread: , LDC3114 , LDC1614 Hello,
Section 8.4.5 of the datasheet mentions that the Rp can be disabled to improve measurement stability. Can you please explain what a more stable measurement means and…
Part Number: LDC1101 Hello team,
I received a question from the customer.
The customer wants to use the LDC1101 in an environment where magnets or solenoids are nearby. In such a case, I think it is necessary to shield the area around the sensor…
Part Number: LDC1101 The LDC1101 has two low power modes: shutdown mode and sleep mode. I understand that no conversions happen in these modes. What is the sensor driver doing during these low power modes? Does it high-Z the coil connections or does the…
Part Number: LDC1101 Now using LDC1101 for the ranging of metal objects, inductors are using ferrite winding inductors. L:70uH, C:1000pF, Rp 56K s without target. Now there are three issues during debugging 1. Close range (<8mm) measurement is normal…
Part Number: LDC1101 I am not getting any LP or Rp Data. Am i missing something? can anyone help me? below is my config param.
int8_t ldc1101_init() { uint8_t chip_id;
// chip_id = ldc1101_readByte( _LDC1101_REG_CHIP_ID ); // if( chip_id != 0xD4…
Part Number: LDC1101 Hello,
We are using the LDC1101 to design a padlock presence sensor.
On a metal bar, there is a hole of 15mm, where the padlock is inserted. The padlock lock diameter can vary between 1 & 14mm. we are looking to put thin coil…
Part Number: LDC1101 Hello,
Is it possible to form the resonant LC section with capacitive probe and a fixed inductor or some coax . The resonant frequency would be modulated with the change in capacitance rather than inductance, the LDC1101 wouldn…