Part Number: LDC1612 Hello.
There are several questions when using LDC1612 to measure the height of different areas on coils and metal planes:
There is a soft magnetic sticker under my metal plane to be measured, which is used to fix the metal plate…
Part Number: LDC1612 Greetings,
We are planning to use LDC1612 for our proximity sensing application.
what is the maximum distance from the metal target it can achieve?
Is it possible to use only one inductor for the operation?
Hope to get continuous…
Part Number: LDC1612 Hello, I have two urgent questions about the use of LDC1612. the first question: I use LDC1612 to measure the unevenness of the metal plane. There are two processes required here. One is to establish the relationship between sensor…
Max,
Yes, you could still use the 40MHz approach without connecting another coil. In this case, you should leave IN1A and IN1B floating. With no coil connected, you will likely receive conversion errors. You could clear and discard the errors on this…
Part Number: LDC1612 我们首次测试,探测距离3mm,天线直径13.9mm。
因结构限制,探测距离要增加到8mm,根据比例计算,天线直径需要做到37.2mm以上,那么检测精度还能跟之前保持一样吗?
你们有类似的探测距离在8mm左右的应用吗?
除了正后方和侧方不能有金属,其他设计还需要注意些什么?
---
Our first test, the detection distance is 3mm, and the antenna diameter is 13.9mm. Due to…
Part Number: LDC1612 Hi Team,
The customer would like to use a PCB coil as the LDC1612 sensor to measure the distance of the PCB coil to a silver-plated mirror.
Issue:
During the movement of the PCB coil (4 mm-20 mm), it is not possible to measure the…
Part Number: LDC1612 Other Parts Discussed in Thread: LDCCOILEVM , Hello,
I am seeing some unexpected output code oscillations which trend in the expected linear direction over any linear displacement. The oscillations appear to repeat every 2mm. The following…
Hello Justin,
could you give a specific absolute accuracy for the high/medium/low resolution.
For example, I use LDC1612 to measure the distance of an object, what are the corresponding values of these three precisions?
looking forward to your reply.
Part Number: LDC1612 There is a question about coil diameter and detection distance.
Can the following two conditions of use achieve similar stability and detection accuracy?
1. Use a 20 mm diameter coil to detect 8mm in diameter;
1. Use a 13.9 mm diameter…
Part Number: LDC1612 Some questions about LDC1612 register configuration. I want to use a function like this: 1. Only use CH0; 2. Full precision conversion time; 3. The INTB Pin generates a falling edge interrupt when the conversion is complete; My register…