Part Number: LDC1612EVM Other Parts Discussed in Thread: LDC1612 , Dear Team,
We are currently working on designing inductive proximity sensor, using LDC1612. for the initial stage, we are planned to work on LDC1612EVM to achieve the target distance of…
Part Number: LDC1612EVM I'm using an LDC1612EVM board. What's the case, if only the red led is constantly ON after pc connection ? Does that mean there's a problem with the board ? Also the GUI is not able to detect the board.
Part Number: LDC1612EVM Other Parts Discussed in Thread: LDC1612 , Hello,
We purchased an LDC1612EVM board and got it working nicely. We took the LDC1612 and coil design from the LDC1612EVM board and placed it on our own custom board.
The issue is we're…
Part Number: LDC1612EVM I am using LDC1612EVM for very small metal detection. When used with USB power, connecting USB cable to PC USB port, It works as expected. Is it safe if I connect external +5V power supply to power lines of USB cables and only…
Good morning John,
sorry fof the late reply, I was out for work. Using Ch1 coil of LDC1612EVM, configuration is the following:
Diveder code: 2 to have a Fref to 20MHz (I'm using only a coil and than Fref have to be < 35MHz)
Idrive code: 19 corresponding…
Thanks John,
As for the object size I mentioned in my previous post, 10 x 0.5 mm is the worst case. I have tested LDC with a best use case, a 3mm round, 1 mm thick Al. object. I measured a good frequency shift of about 22 KHz at 2 mm distance, with the…
Part Number: LDC1612EVM Other Parts Discussed in Thread: LDC1612 I am using LDC1612EVM board rev B. Once I upgraded wrong firmware, it stopped working. Got solution from Ti Technical support. As per advise, shorted PUR and VUSB pins (R6 and C29). Board…
Part Number: LDC1612EVM Hello,
I am having trouble establishing a connection between MSP430 on LDC1612EVM. I am attempting to use the USB virtual serial port communication interface of MSP430 on LDC1612EVM with my own python script to poll the sensor data…
Part Number: LDC1612EVM Hi, I am using the LDC1612EVM for linear sensing application. The coil being used has the following parameters attached below:
The sensor inductance sampled value has a baseline at 58uH and raw data value of 6413055. Frequency set…
Part Number: LDC1612EVM Other Parts Discussed in Thread: LDC1612 Hi Team,
Our customer is using LDC1612EVM. According to the customer,
While using Excel_FEMM_v1p28.xlsm for Inductor calculation , I used coil data of the sample coil PCB supplied with LDC1612EVm…